Hello Chihiro,
Please refer some of the threads and key observation/recommendations.
Do you see this issue on a specifc board or on multiple boards. is there a specific use case when the issues happens?
Have you considered all the design guidelines or…
Part Number: AM3354 Hi AM335x Champ
Can you please let me know if AM335x also supports High Security device?
A customer would like to implement the security features like secure booting.
Also let me access HS SDK for AM335x.
Thanks.
Regards,
Jack
Part Number: AM3354 We are looking to implement secure boot for an existing design using the AM3354 processor. I understand that an NDA is required to obtain the necessary documentation for implementing secure boot, what is the process for getting the…
Part Number: AM3354 Hello there,
Reading the SPRS717F doc I cannot find the resistance value of the internal GPIO pull-up resistors (and pull-down, if possible to configure for a GPIO).
So when internal pull-up is configured for an input, what values…
Part Number: AM3354 We have thermometers connected to AIN0 to AN2 as single-ended .
The full scale range of the ADC is 0 to 1.8V.
It's 1.8V on both VDDA_ADC and VREFP while VREFN is connected to VSSA_ADC on the board.
However it seems that ADC only…
Part Number: AM3354 Dear Sir,
In our board, USB0 is device mode and the role of USB0 is console port and firmware upgrade in our board.
The USB0_ID can be left unconnected(it is GND in our borad) or should be left unconnected?
Part Number: AM3354 Hi AM335x Champ
My customer found an handled fault issue when they added gpio_direction_output() code in set_termios() of driver/tty/tty_ioctl.c file.
...
#define GPIO_TO_PIN(bank, gpio) (32 * (bank) + (gpio)) #define FLOW_CONTROL…
Part Number: AM3354 Other Parts Discussed in Thread: TIDA-01568 Hi AM335x Champ !
Could you please let me know how to get the uboot patch for TIDA-01568.?
A customer would like to design AM335x board without PMIC.
They are seeing the boot failure issue…
Part Number: AM3354 Hello All,
We are using AM3354 processor for our application, We need some default Linux Bootable Images for AM3354 for testing purpose. From where I can download the default images?
Is there any default linux image available for…