Part Number: AM3356 Tool/software: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1341607/am3356-cpm-isr-miss-when-the-irt-and-rt-mixed
This thread has been locked but the bug was not fixed.
Let's continue in this thread.…
Hi Chippy,
I recommend checking page 2 of the AM335x datasheet :
It mentions: – Up to Two Controller-Area Network (CAN) Ports – Supports CAN Version 2 Parts A and B
Best,
Mahir Kaheri
Hi All,
Additional inputs
Customer is asking if there is a way their firmware can tell if the CPU is AM3352 or AM554D80 or Z100? Like a register to read from?
Please refer to the below register
Data sheet reference:
www.ti.com/.../am3352.pdf
3 Device…
Hello, Thanks for the confirmation. I recommended you try to debug the gpio_keys.c driver, so at least you can see the variable values when the issue does occur. There are a few functions that covers the event generation.
https://git.ti.com/cgit/ti-linux…
Hi Katsuyama-san,
Takeharu Katsuyama said: 1. These patches are valid or invalid?
As you said, the first patch (1/2) is already in the kernel, so it is valid. I will review the second patch and get back to you.
Takeharu Katsuyama said: 2. The mechanism…
Part Number: AM3356 On SITARA the ethernet port interface name is "eth0" and "eth1" (in dual MAC mode).
I have a problem with the "eth1" name, because we already have some other network interface over USB for which we have already…
Part Number: AM3356 Tool/software: We used the chip am3356, and we connected a wifi module through the SDIO interface. In the process of speed measurement, we found that the rates of 11a and 11n were very poor. The manufacturer of the wifi module required…
Part Number: AM3356 Hi TI,
I am investigating micros/DSP for a new device for multichannel audio transfer. The device will connect to a smart phone or PC and transfer multichannel audio data via USB.
We would like to use isochronous transfers.
Are you…
Hi Andy, Apologies for the delay. We had been suspecting the FIFO delay calculations to cause the issue here and it seems like this is a partial cause of the issue. Due to some timing related issue the whole PPM packet is not being sent by the device, and…
Part Number: AM3356 Hi, My customer wants to use DMA for UART3 transfer. OS is SDK Linux. Q1) Could you tell me how to enable DMA for UART3? Q2) Can UART3 with DMA support up to 1Mbsp? Thanks and regards, Koichiro Tashiro