Part Number: AM3517 Other Parts Discussed in Thread: AM5708 , AM5706
Tool/software: Linux
Dear All,
We are planning to use the AM3517 SOC for one of our Application in which we have below query so please help us to solve this.
Can we read BT656 supported…
Part Number: AM3517 Tool/software: Linux Hello,
We are working on migrating from an older version of Yocto project Daisy(1.6) to Rocko(2.4).
We are able to build meta-ti successfully and generate the following components for am3517-evm.
1. MLO(53 Kb) …
Part Number: AM3517
Hi Experts, Could you please let me know about the VIH(min) for USB0_VBUS? Does AM3517 work if USB0_VBUS is 3.3V?
According to the datasheet in 5.1 Absolute Maximum Ratings, USB VBUS pin (usb0_vbus) (max) is 5.5V. I believe that the port…
Part Number: AM3517 I am not having any success trying to connect the VS2008 debugger to my WEC7 device.
I am not seeing any BOOTME traffic coming from the AM3517. Is there some EBOOT option that will enable/disable the BOOTME broadcast? (I am not finding…
Part Number: AM3517 Tool/software: Linux We are experiencing challenges getting the synchronous type of transactions. The AM3517 is implemented on a COTS COM board and the GPMC bus interfaces with a Xilinx Spartan 6 FPGA. The total chip selects that are…
Michael,
thanks for asking...we TI focus on Linux and Witekio (www.witekio.com) has ported some Microsoft OS to our devices. Please check with Witekio.
Part Number: AM3517 Hi Experts, Could you please let me confirm whether AM3517 works as a USB device if VBUS Low-power Port voltage 4.4V (min)? I believe that it works. Thank you very much for your check. Best regards, Hitoshi
Part Number: AM3517 In the following E2E post
https://e2e.ti.com/support/processors/f/791/t/181498?pi316653=2
There are a number of broken links. The b roken links that I am interested
http://e2e.ti.com/members/1791104/files/nand_5f00_prefetch.tar.gz…