Hello,
B.C. said: Would there be any issue with your system using this capacitor approach on RSTN instead of using the RSTOUT_WD_OUTn output of AM3874 ? This would allow the CDCM61002 to be free run as long as power is applied and independent of AM3874 …
Part Number: AM3874 Hello,
I would like to put my app to sleep for 100 microseconds. I've used usleep function but I've noticed that it sleeps for about 200 microseconds. I wrote the following program to check what's what:
#include <stdio…
Part Number: AM3874 Hi, My customer is using AM3847 and reported display image corruption. Here is their usecase: - RGB data are in DDR3 - RGB data are transferred from DDR3 to HDVPSS(VPDMA =>GRPX=>HD_VENC_D) to LCD output. - Cortex-A8 writes…
Part Number: AM3874 Hi, My customer is using both AM335x and AM3874. He uses UART TXFIFO_LVL register in AM335x and found the register is missing in AM3874 TRM Table 24-9. As far as he tried to use the TXFIFO_LVL register on silicon, the register is…
Part Number: AM3874 Hi,
My customer is using AM3874CCYE100 and they do the Hi-Pot test( 1850 VAC for 2 seconds ) at production line.
They found the fail rate is 6% (Total units run: 100 / Total fail quantity: 6) and then DVI ouput unstable or NO DVI output…
Part Number: AM3874 Hello, I'm planning to design a small board that receives Gigabit ethernet data and saves the data to CFAST 2.0 Compact Flash card using the SATA interface. In the event that main power is cut I need to close the data file on the Compact…