Part Number: AM3892 Tool/software: Linux Hi,
The AM3892 Datasheet specifies that the resistance of the HDMI_EXTSWING line should be 6.8 kohm.
But, the EVM Board is connected at 5.9 kohm.
Please let me know which is correct.
BR,
Hi Pallabi,
VxWorks has a nice little search engine @ https://bsp.windriver.com/bsps/product/vxworks_6-9 - below are the search results for TI processors support.
The assumption is that whatever bootloader is needed, it will come with VxWorks 6.9 (We…
Part Number: AM3892 Customer using EZSDK 5_04_00_11
The problem they have is that CPU does not receive an interrupt of reception of Ethernet packet on EMAC0 port.
During it, CPU can send a packet through EMAC0. The problem is only on receive direction…
Other Parts Discussed in Thread: AM3892 Hello,
We are using ARM AM3892 Sitara processor in our customized design,
We have two Boot mode option,1) NAND Boot, 2) SD Boot,
We have configured to SD Boot mode in our design,
We are getting SD clock from ARM…
Other Parts Discussed in Thread: AM3892 Hello
where can i find details of the applications that comes with EZSDK for Sitara AM3892 (codec application...) I need application the can :
-store audio input on SD memory,
-store data coming from ethernet link…
Hi,
Just an confirmation about the errata Advisory 2.0.68. Advisory 2.0.68: Continuous Writes From Cortex-A8 Occasionally Starve Other Requestors for DDR Bandwidth .
We would like to confirm if the above Errata is FIXED in the latest Silicon Revision 2…
Other Parts Discussed in Thread: AM3892 , CCSTUDIO I'm writing a BSP for an SD Card driver, and encountered an issue which is preventing me from reading data from the SD Card.
The SD Card driver is attempting to read the SCR from the card using CMD51…