Hello
where can i find details of the applications that comes with EZSDK for Sitara AM3892 (codec application...) I need application the can :
-store audio input on SD memory,
-store data coming from ethernet link on SD memory
-read input IO …
Hi Sir,
i am using customized board based on TI8168 board. Here
1. i did not find c code for DDR2 stuff in board-ti8168evm.c.
Is this correct place to check Low level initialization of DDR2 interface.
If not then which is the right place or right…
Hi,
We need some advice regarding AM3892's GMII connection.
Our customer board has two AM3892 connected each other through GMII.
We would like to know if the AM3892 EMAC support MAC-to-MAC protocol and is it OK connecting two devices through GMII…
Hello,
I have custom board based on am3892 revision 2.0 TI processor. I know there was some problems with booting via UART in previous revision.
Is it possible on 2.0 revision processor. Is there any booting via UART guide for this processor?
…
Other Parts Discussed in Thread: SYSCONFIG In the GPIO section it states:
Note: General-Purpose Input/Output (I/O) pins can also serve as external interrupt inputs.
In the interrupt section it is indicated the following:
7 NMI External Pin
96…
We are using CCS 6.0.1.00040 and a XDS200 USB Emulator pod to communicate to a AM3892 on a custom board. We're currently attempting to initialize our DDR3 interface (EMIF 0 only) using the procedure described here: http://processors.wiki.ti.com/index…
Hello,
We have custom board based on TI AM3892 processor. I would like to use USB device with my board. HID (mouse, keyboard) and usb-storages for the first.
During startup everything seems to be okay, but when we trying to plug-in mouse or flash…
Hi,
We managed to solve this issue. The reason was GPMC_CONFIG1 register for cs1 and cs2 not configured properly. I've copied those register's configuration from cs0 settings and now it works.
Best regards,
Anton
Hi,
I have custom board based on am3892, i'm trying to run Android but during boot 'recovery' is called. Have you got any clues about this issue?
Here I provide full log:
Terminal log file Date: 04.02.2013 - 8:43:28 --------------------------…
Other Parts Discussed in Thread: MSP430F2132 Hello,
I have custom board based on TI AM3892 processor. We've managed to run Linux + Arago FS on board through the agency of E2E Community and espesially Pavel Botev. The board's design is very similar to…