Other Parts Discussed in Thread: AM3892 Hi,
I have custom board based on am3892, i'm trying to run Android but during boot 'recovery' is called. Have you got any clues about this issue?
Here I provide full log:
Terminal log file Date: 04.02…
Other Parts Discussed in Thread: AM3892 , SYSCONFIG In the GPIO section it states:
Note: General-Purpose Input/Output (I/O) pins can also serve as external interrupt inputs.
In the interrupt section it is indicated the following:
7 NMI External Pin
96 GPIOINT0A…
Other Parts Discussed in Thread: AM3892 Hello,
I have custom board based on am3892. I'm trying to boot Linux PSP using u-boot via SD card, unfortunately it doesn't work.
We suggest there could be some problems with RAM on board. I've tried to boot…
Other Parts Discussed in Thread: AM3892 , LINUXEZSDK-SITARA , PMP Hello,
I have an custom board, based on am3892 TI processor. I'm trying to boot Linux via SD card, using Linux PSP Release 04.00.02.14.
I managed to load u-boot and trying load Linux following…
Other Parts Discussed in Thread: AM3892 Hi,
I have an custom board based on TI am3892 processor. I'm trying to load linux via SD card. U-boot starting successfully, linux kernel image loading to RAM and then kernel booting starting. But during linux kernel…
Other Parts Discussed in Thread: AM3892 Hello,
I have an custom board, based on am3892 TI processor and I'm trying to install Android (boot from SD card) on it following guide on TI website.
http://processors.wiki.ti.com/index.php/Android_am389x_b…
Other Parts Discussed in Thread: AM3892 Hi.
1.I want to program the FPGA through the ARM processor, where ARM is the master. The FPGA configuration data is in a flash connected to the ARM. I am planning to connect the AM3892 processor through GPMC to the…
Other Parts Discussed in Thread: AM3892 Greetings,
I'm thinking of starting an ARM server design based on the AM3892 w/SATA. Any advice on such a project? Are there reference designs available?
Thanks,
FM
Hi,
We want to measure 1 Gigabit traffic for our new test equipment. When I see PSP_04.00.00.13 performance
guide with iperf , it shows approximately RX 600Mbit and TX 750Mbit with CPU 1GHz
and DDR3@800MHz. If we increase CPU speed 1.35 or 1.5GHz and max…
Other Parts Discussed in Thread: AM3892 Hello,
I have custom board based on am3892 revision 2.0 TI processor. I know there was some problems with booting via UART in previous revision.
Is it possible on 2.0 revision processor. Is there any booting via…