Other Parts Discussed in Thread: AM3894 , CCSTUDIO Hello all.
I have custom board with AM3894 and DDR3
DDR3 (size 1GB, two chips K4B4G1646B-HIH9 x16 as one space x32) connect to EMIF0, EMIF1 not use.
default Gel-file TI816x_DDR3 don't work
Calculated…
Hi,
Booting device with microsd. U-boot loading is successful, but uImage not loading.
U-boot error: Verifying Checksum ... Bad Data CRC ERROR: can't get kernel image!
Try booting uImage with TFTP, all right. Microsd create with tool: mksd-ti816x.sh…
In AM389x Techical Reference Manual SPRUGX7C, Table 7-64 shows that three bits 2-0 (ADDR_CMD_CFG) are used to configure Address/Command I/O pad. The technical reference manual shows that the three bits can have a value in the range 0-7h. But, I cannot find…
Other Parts Discussed in Thread: PMP Loading kernel stop on "Waiting for root device /dev/mmcblk0p2..."
I am not use card detect pin on CPU (card detect pin pullup 10KOm on 3.3V).
My boot log:
Linux version 2.6.37 (admin@admin) (gcc version 4…
Dear All,
as they say here.
"Note-3: TI81XX PCIe hardware does not support hot plug and if an EP directly connected to the TI81XX RC goes down (e.g., powered down or disabled), the complete PCIe h/w initialization needs to be repeated and PCI enumeration…
Other Parts Discussed in Thread: AM3894 Hi! All
Now, I try to use 2 port Ether(eth0,eth1) on AM3894 with Ubuntsu.
But, I can not succeeded to use 2 port Ether.
Someone have been able to succeed to use?
if you have already succeeded to implement, please…
Other Parts Discussed in Thread: AM3894 Hi all,
I used NAND flash(MT29F32G08CBADAWP-D) on AM3894. I referred TRM into GPMC chapter to know the calculations in each registers of GPMC_CONFIG1_i - GPMC_CONFIG7_i .
After that I could R/W the NAND flash successfully…
Other Parts Discussed in Thread: AM3894 Hello,
I have a problem with my AM3894 processor. I'm loading an u-boot in memory at location 0x81000000 and I set the PC to the same address.
When I click start, the PC move to 0x00020080 and stay there forever…
Other Parts Discussed in Thread: AM3894 Dear sir,
My problem is as below.
During power on/off test, it will be happened 20~40 power on/off test.
The phenomenon is after power on, it seems booting completed, but it is not connected Ethernet.
So I tried…
Other Parts Discussed in Thread: AM3894 , LM10010 Hello,
I am using AM3894 in my design and implemented AVS feature using GPIO feature. Instead of the implementation in Spectrum DM8168 EVM, I used a TI VID IC, LM10010 which also uses the same GPIO pins…