Part Number: AM4372 Hi,
For USB device mode of AM4372, what is USB_VBUS valid threshold voltage?
In datasheet, it seems to be 4.4V.
However, USB host can supply 3.3V now and in this case, AM4372 works well as USB device mode.
Is there any problem?
Thanks…
Part Number: AM4372 Other Parts Discussed in Thread: SYSBIOS Hi everyone,
I am currently using Uart0 and Uart2 to communicate with 2 different devices.
This is the configuration of the Uarts:
off_board_uart0_pins_default: uart0_pins_default { pinctrl…
Part Number: AM4372
Hi,
We are using yocto 07_03_00_005 PSDK version and it supports 5.10.100 kernel. We want to know, What is the latest LKML version supported for AM4372. Please let us know.
Thanks,
M.Mahesh.
Part Number: AM4372 I'd like to design a system based on the AM4372 SOC.
I'd like the GPMC bus to be clocked with an external oscillator that has a frequency of 43.75 MHz.
Does this device support that ?
Part Number: AM4372 Hi,
I am using TI SDK "proc-sdk-secdev-am437x-hs-evm-01.06.00.05" to build the MLO file but It doesnt work(i.e. no serial output).
Could you provide more explanation how to verify the address "ISW_LOAD_ADDR" passed to the…
Part Number: AM4372 I have a Jenkins build setup to create an USB boot image and USB boot is not working consistently from the USB device. In other words, same image written to kingston datatraveler G4 16 GB USB, this works, but board doesn't bootup i…
Part Number: AM4372 Hi TI
A customer is testing Power Saving Mode Entry and Sleep with RTC. Their system is powered by connecting PC and USB, and aims to wake up via USB in a sleep state. They are currently having a hard time waking up through USB event…
Hi Kanae,
After further reviewing the DCAN code on the AM4372 in the DCAN community driver the CTRL_DCAN_RAMINIT process is being done in the Linux driver. There are commit messages in the driver indicating that this step is required.
Best Regards,
Sch…