Part Number: AM4376 Hello,
We are using AM4376 processor with RT Linux. We are using processor SDK ver 8.03. Till date we have compiled the code and developed an application on it. We are using .network files for DHCP configuration. But then it becomes…
Part Number: AM4376 Hello,
i am working on TI Linux sdk 8.02 with ethernet related services and PRU is being used for ethernet interface.
i am typing command arp -a but it does not provide any ip list connected over network. what could be the reason…
Gaurav More said: There it also has the Linux Installer named "PRU-ICSS-EthernetIP_Adapter-01.00.04.11-Linux-x86-Install.bin"
This is installer for Linux environment (Linux PC) for debug or building the application.
As we already mentioned for…
Part Number: AM4376 Hi AM437x Security Champ
Could you please let me access Crypto TRM continously?
My account can not access it since it expired.
Also allow me to access AM335x Crupto TRM if available, My customers trying to activate Security Features…
Hi Lukas,
I used AM437x USB client boot many years ago, I don't think you need to adjust the ENTRY ADDRESS.
I will try to test it again on AM437x EVM and get back to you.
Part Number: AM4376 Hi Support Team,
Is my understanding correct that AM437x has two types of WDT modules, WDT0 and WDT1? From the datasheet, it looks like there is only WDT1, so in the TRM, there are enable settings for PRCM_CM_WKUP_WDT0_CLKCTRL and…
Part Number: AM4376 Hello,
I am using AM4376 processor for our product development. We are using RT Linux for the development. While going through the implementation of secure boot, we referred processor_SDK _build_install _guide.pdf.
Followed the instruction…
Part Number: AM4376 Hi
My customer would like to implement the high security features like secure boot on top of AM335x, AM437x, AM64x.
Please give me some useful guide regarding Sitara Security Feature support overview on AM335x, AM437x and AM64x.
Thanks…
Part Number: AM4376 Hi to all experts out there,
I would like to know something regarding the right termination for unused DDR3-lines.
Within the datasheet it is written section 5.12.8.2.1.3.1 Schematic
That it is recommended to "tie off the DDR_DQS…
Hello Kanae,
Thank you.
Based on the inputs i assume that customer now understand the clock configuration.
Kanae said: In a linux environment with TISDK 7.3.0.5, when I boot WDT1 (echo 1 > /dev/watchdog0), the supply clock is CLK_RC32K. I would like…