Hello Zhicheng,
We have detailed brainstorm on this issue and have identified the reason why the ROM code is unable to detect the newly written MLO file after certain amount of reboot.
The reason is that the fat driver part of the eMMC boot functionali…
Part Number: AM5716
Hi experts
Recently, we encountered that the NIC issue of the AM5716. If we continue to down/up the network card for one day, the kernel will report the following error(ps. The network card is transmitting network data during down…
Part Number: AM5716 Hi experts
Recently, we encountered that the RS485 of the AM5716 issue, when we use the close function when sending and receiving data and when it is opened again, the RS485 port cannot be used. It can be used if it is closed when not…
Part Number: AM5716 Been going through the documentation, but I only see the minimum for the configuration using ECC, but not the min or max for configurations without it.
Keerthy,
If remove the no-1.8-v from the MMC node, it will support HS200 eMMC? and what is the frequency of HS200? can it output 200MHz/192MHz eMMC clock?
&mmc2 { status = "okay"; vmmc-supply = <&v3_3d>; vqmmc-supply = <&v3_3d…
Parth Nagpal said: applying
Hi Parth,
Thank you.
Can you let me know to apply this patch ?
directory
the target file to be applied
exact command to apply this patch
Thank you for contacting us. The WDT issue has not been resolved. However, I was able to achieve my goal by implementing WDT and WDLY myself.
thank you.
Part Number: AM5716 Hello,
The SDK version is 06.03.00.106, Change uart3 pin from uart2 in hardware_ Rtsn/C28, uart2_ Ctsn/D27, switch to mcasp5_ Axr0/AB3, mcasp5_ Axr1/AA4, The software has made the following changes: Mux in uboot_ In data. h, added {MCASP5_AXR0…