Part Number: AM5749 hello I'm trying to create an SD card to boot an AM5749 board. Previously, I was able to boot the SD card by entering the URL provided by PROCESSOR-SDK-LINUX-RT-AM57X. Below is that URL.
software-dl.ti.com/.../Overview_Getting_Started_Guide…
Part Number: AM5749 Hi team,
At this thread, there is description of " We checked internally and our next release with support for Kirkstone Yocto for AM57x would be SDK 9.1 based and planned release timeframe is end of Nov this year . ".
However…
Part Number: AM5749 Other Parts Discussed in Thread: TLV320AIC3104EVM-K , AM5728 On the AM5749 I have performed pin muxing to change pin vin1a_d6 to pr1_pru0_gpi3 (attaches to external push button), and gpio4_8 to pr1_pru1_gpo4 (attaches to external LED…
Hello Tay,
Sorry for the severely delayed response, this thread was assigned incorrectly and fell through the cracks..
Anyhow it seems like you have progressed from this based on this thread https://e2e.ti.com/support/processors-group/processors/f/processors…
Can't you take the timestamp from TSC in ISR serving FPGA IRQ and another timestamp in ISR serving EDMA completion interrupt?
The difference between the 2 timestamp (TSC freq is the same as DSP clock) can be used to convert to time for transfer latency…
Part Number: AM5749 Other Parts Discussed in Thread: AM6252 Hi
We are in process of selecting a processor with inbuilt 3D-GPU. and 2/4 cores , Which can give simultaneous output data on two Monitors ( XGA- 1024×768, and VGA 768x576 )
We have selected…
Hello Romain,
Romain Naour said: What about the content of meta-ti for Kirkstone, especially the common-csl-ip package ?
There will be updates to meta-ti as part of the Kirkstone migration. that be part of the SDK 9.1 release. Suggest waiting for the…
Part Number: AM5749 Hi,
I have a custom board based on AM5749 Sitara processor. Everything works fine when booting from SD card. The problem occurs when eMMC is used as boot device (when SD card is not present). Sometimes the boot fails and I get this log…
Part Number: AM5749 Hi Dears,
I am using the TMS320C66x DSP CorePac of this SoC.
As data exchanges are required with the Dual Cortex-A15, we retained the IPC stack solution.
Seems that stack is only available on TI-RTOS (no baremetal version is available…