Part Number: AM5749
Hi,
I am currently working on disabling the unused cores on AM5749. We have a baremetal application using Processor SDK RTOS. (We didn't use the RTOS component). My application runs on Cortex A15 _0 and it is the only core that needs…
Hi Divyesh,
Sorry for the late reply.
For the profinet application, the sdk provides an inbuilt evaluation library for the snmp stack. The snmp_core_stack project needs to be built only if you want to rebuild/modify the stack.
So, If you want to rebuild…
Other Parts Discussed in Thread: AM5749 Hello support!!
I'm using AM5749 custom board with PROCESSOR-SDK-LINUX-RT-AM57X 05.03.
Which driver I should use for a work from user space with hardware decoder H264 without display connection.
B.R, Oleg
Hi,
Since this is a duplicate post, we will close this one and actively work on this in the other post. Please refer to the below post going forward.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1074016/am5749-am5749-tmdsidk574…
Part Number: AM5749
Hello,
Using the Linux kernel 4.19-rt provided by the TISDK 6.03, I was able to use a GPS device connected to the uart4 of the AM5749 device (custom board). As a basic test I'm using gpscat, gpsmon or gpsctl to open the /dev/gnss0…
Part Number: AM5749 Hello,
we have custom board based on AM5749 processor.
I know how to do it on my development board with SDK (simply make install).
We have our own ipk-repository and successfully upgrade our application from it. This solution is the…
Part Number: AM5749 Other Parts Discussed in Thread: BEAGLEBOARD-X15 Hi,
Just sharing study note. I saw a unsolved thread on forum. Thus, I write down the note for someone gets the same issue. I will close the thread tomorrow.
Board: TMDSIDK5749 (I guess…
Hi Oleg,
IVA-HD does not have any Linux driver representation, it is all controlled from one of the remote processors (IPU2 pre-dominantly).
regards
Suman
Hi Miyazaki-san, Do you have access to CCS? Can you please attach JTAG and checkout where exactly is the ARM core executing? Could you check if the execution has entered SPL?
Best Regards, Keerthy
Hi,
Please find the schematic. It's the schematic for our next board revision. As my post explained, we did the tests with a prototype (our current board revision and an evaluation module with the Ethernet switch on it). So the schematic for our prototype…