Hi,
khoosen Yu said: Booting Error-20220925.txt
Is this the complete logs? Does it ever come out of the loop and proceed further?
khoosen Yu said: After this modification custom board boots more(?) time. :)
I am little confused with the statement here.…
Part Number: AM5749 Is there a way to view the contents of L1 and L2 cache on the ARM Cortex-A15? I don't see any ability to do this in code composer studio for this particular processor.
Is there any way to guarantee or overwrite the contents of…
Part Number: AM5749 Other Parts Discussed in Thread: BEAGLEBOARD-X15 , AM5728 Hi Dear.
Recently I Download the TI-Processor-sdk-linux-am57xx-evm-08_02_01_00 and install successfully in VMWare-Ubuntu 18.04LTS(64bits).
I success on "make linux", "make u-boot…
Hi Divyesh,
Sorry for the late reply.
For the profinet application, the sdk provides an inbuilt evaluation library for the snmp stack. The snmp_core_stack project needs to be built only if you want to rebuild/modify the stack.
So, If you want to rebuild…
Other Parts Discussed in Thread: AM5749 Hello support!!
I'm using AM5749 custom board with PROCESSOR-SDK-LINUX-RT-AM57X 05.03.
Which driver I should use for a work from user space with hardware decoder H264 without display connection.
B.R, Oleg
Part Number: AM5749
Hello,
Using the Linux kernel 4.19-rt provided by the TISDK 6.03, I was able to use a GPS device connected to the uart4 of the AM5749 device (custom board). As a basic test I'm using gpscat, gpsmon or gpsctl to open the /dev/gnss0…
Hi,
Since this is a duplicate post, we will close this one and actively work on this in the other post. Please refer to the below post going forward.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1074016/am5749-am5749-tmdsidk574…
Part Number: AM5749 Other Parts Discussed in Thread: BEAGLEBOARD-X15 Hi,
Just sharing study note. I saw a unsolved thread on forum. Thus, I write down the note for someone gets the same issue. I will close the thread tomorrow.
Board: TMDSIDK5749 (I guess…
Part Number: AM5749 Other Parts Discussed in Thread: PMP , AM5748 Hi, All: This is note for SATA boot with clone of am5749_IDK. I saw some unsolved thread on forum. Thus, I write down the note for someone get the same issue/hole/trap. I will close the thread…
Hi Oleg,
IVA-HD does not have any Linux driver representation, it is all controlled from one of the remote processors (IPU2 pre-dominantly).
regards
Suman