Part Number: AM625 Good day,
We are using custom am625 sk evm for our project . In this we tried to boot the emmc from sd card. but while untarring the .xz file I'm facing the issue as in image. herewith, I have attached my boot procedure document…
Part Number: AM625 Hi, My customer measured 64bit TRNG generation time on both SK-AM62x EVM and their custom board. They found there were big differences. SK-AM62x : 500msec Custom board : 50usec Are there any factors which may impact to TRNG generation time…
Part Number: AM625 Hi Expert,
Customer said that the circuit is based on the BeaglePlay without any changes, but it cannot boot.
There are six boards with the same situation.
Do you have any suggestions on how to debug?
Thanks
Daniel
Part Number: AM625 Hi, My customer is considering to use QSPI-NAND. The memory datasheet is attached. MX35LF1G24AD, 3V, 1Gb, v1.2.pdf As you can see in page#5, #6, the device needs the host side to support 8-bit ECC/544-byte operation. And page#27 describes…
Part Number: AM625 Hi Team,
As per our requirement ,
query1:we need eMMC in back-up boot ,primary boot as USB(DFU mode).Is there a possibility?
query2:
We had kept USB(DFU) as primary boot, SD card as back-up boot mode. It works as expected provided…
Part Number: AM625
Hi,
What is the default CPU frequency ( form dts "opp-table") in am62x-sk-evm u-boot?
is any mechanism in u-boot to choose frequency scaling governor like in kernel?
Regards,
Gireesh Hiremath
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62B-P1 I would like to do Ethernet booting on the am62-evm board, I don't know how to do it and if there is any documentation available. If I want to have sd as the primary boot and ethernet as the…
Part Number: AM625
Hello,
we experienced the following Oops a few times, using TI Linux Kernel 09.02.00.008 on custom hardware while accessing the eMMC device.
[ 31.377291] Unable to handle kernel paging request at virtual address 0000fffffc386a14
…
Part Number: AM625 I'm trying to use LVDS on our custom hardware featuring a AM6254. When using the tisdk-default-image build with the ProcessorSDK 9.01.00.x the Display is working and the kernel module tidss.ko is loaded as expected.
When I build…
Hi Alan,
Alan Wen said: We got a failed message as below that means pins MOSI (D1) and MISO (D0) aren't connected.
Can you please check the below link to a working reference and see if you can make it work on your end. Could be that something with the…