Part Number: AM62D-Q1 Hi,
I’m looking for detailed documentation or reference material related to DRU (Data Routing Unit) on C7x. I haven’t been able to find sufficient information—could you please point me to the relevant documents or guides?
In…
Part Number: AM62D-Q1 Hello TI experts,
I want to transfer data from McASP via cyclic DMA. Do you know is there any limitation on AM62D to set the number of DMA periods? Can I configure DMA so that it only copies the word size(16 or 24bits) data ?(I…
Hi experts,
Thsi is additional information.
Operation is assumed at 3733 Mbps. The specification values on the READ side (AM62D-Q1) are strict. Since LPDDR4 does not specify values equivalent to the setup and hold times of normal signals, they refer…
Part Number: AM62D-Q1 Hi,
I need to use __atomic_swap available in c7x.h on C7x core. It is mentioned in available documentation but not describe in detail. I am looking for this detailed description. I can guess how to use by it looking at signature…
Part Number: AM62D-Q1 Tool/software: Hello hope you are doing well. I have a question regarding the AM62D:
Does it have a display interface that is multiplexed with the GPMC pins?
We want to have the ability to connect a display and looking…
Part Number: AM62D-Q1 Other Parts Discussed in Thread: SK-AM62A-LP Hi experts,
Q:Could you please tell me how to write and boot the SBL null built by the "AM62A SDK" on the AM62D evaluation board? Alternatively, could you explain how to write and boot…
Part Number: AM62D-Q1 Hi experts,
My customer has started designing a board using the AM62D. They are conducting PI (Power Impedance) simulation. For Core 0.85V, in the high-frequency range above 10MHz, the target value cannot be achieved due to the…
Part Number: AM62D-Q1 Other Parts Discussed in Thread: AM5716 I will use the MCSPI in master mode to connect to a peripheral. I wish to use the start-bit (SBE) feature (register MCSPI_CH0CONF bit23 (SBE)) where an extra bit is added to the transmitted…
Part Number: AM62D-Q1 Hi, I am trying to replicate the cycle counts reported in DSPLIB user guide performance section. I have a couple of questions. 1)Using examples in the SDK release, I am able to almost match the cycles given in the document when I…
Part Number: AM62D-Q1 Hi experts,
I am planning to use USB-DFU for tasks such as booting SBL_NULL for debugging and launching prototype images. Could you please clarify which binary should be loaded when I want to boot SBL_NULL via USB? Reference: U…