Part Number: AM6421 For the am64xx, which is the boot uart, uart0 or the mcu_uart0?
During boot how does the rom code determine when to move from primary to secondary boot?
We are planning on having nand as primary and uart as secondary boot.
Looking…
Part Number: AM6421 Hi,
We are using Industrial Communication SDK V9.00.00.3 on Ethernet Ip Adaptor Discrete IO profile Example.
Requirement was to provide to our customer both implicit and explicit messages.
1. Implicit Messages -- works…
Part Number: AM6421 Other Parts Discussed in Thread: SYSCONFIG Hi,
We want to have below combination for our custom board on Ethernet Interface with DP83822 Phy
- 2 No's Real Time Industrial Ethernet on PRG1-PRU0 and PRG1-PRU1 as MII interface(WITH COL…
Narasimha Rao .
you are getting these messages while debugging or just running the example ?
In case of running example we will need more information to be able to analyze:
board type on which customer is trying to run example
SDK version which he…
Part Number: AM6421
Hi,
Can we use RMII interface for CPSW Ethernet port using DP83822 on AM6421 on Linux.
Below are our connections between AM6421 and DP83822.Please confirm if it will work
PRG0_PRU1_GPO18 (P5) on AM6421 - PIN…
Part Number: AM6421 Hi,
Background: Ethernet-Ip Adaptor Application on AM6421 using Generic Device Profile. For Explicit messages
Issue: When using Generic device profile Ethernet-IP Adaptor Application on R5F0_0 we are unable to receive IPC messages…
Part Number: AM6421 Other Parts Discussed in Thread: SYSCONFIG , Hello TI Team,
I am using AM64x MCU SDK version mcu_plus_sdk_am64x_09_01_00_41 and trying to access GPMC peripheral as NOR type memory device in 16bit non-multiplexed mode. When I am trying…
Part Number: AM6421 HI,
We want to use below main Domain GPIO's in MCU (R5F1_0)firmware on Linux.
(D16) UART1_CTSn.GPIO1_58
(E16) UART1_RTSn.GPIO1_59
We are able to remote boot the R5F1_0 firmware successfully. But the above GPIO's are not…