Part Number: AM6421 Team,
Linux OS is required for the PC to flash the AM64x via USB. Is it possible to use Windows OS as well?
Which dfu-util version should work? Maybe all versions?
Is there an alternative way to boot via DFU?
Are there prebuilt-images…
Part Number: AM6421 Team,
as you can see below there are eMMC boot partitions
https://www.micron.com/-/media/client/global/Documents/Products/Technical%20Note/NAND%20Flash/tn2918.pdf
main question:
- How eMMC boot partitions can be used?
- Do we support…
Part Number: AM6421
Hi Ti experts
In our project, we are using your AM64x SKEVM boards. For development purposes, we need to use BOOT over Ethernet functionality.
As a reference image for testing I'm using your default image available in SDK from the…
Part Number: AM6421
Hi Team,
Our customer would like to know the complete part number of the AM6421 with Pre-integrated Stacks Enabled. Table 10-1 of the datasheet shows the device nomenclature but the product page only shows AM6421BSDGGAALV and AM6421BSEFGAALV…
Hi,
1.VDD_ Core can use 0.75V and 0.85v power supply. What is the difference between these two voltages? What is the effect of choosing different voltages?
2.Can VDD_CORE, VDDR_CORE, VDD_MMC0,VDD_DLL_MMC0, VDDA_0P85_SERDES0, VDDA_0P85_USB0 all be powered…
Part Number: AM6421 Other Parts Discussed in Thread: AM6442 , Hi,
I need some encryptions algorithms in my design for communication security. Is cryptographic engine (AES, SHA, DES, TRNG etc.) is a standard feature in AM6442 and AM6421 ? When should I go with…
Part Number: AM6421 Hi TI,
Is RGMII Interface supported for EtherCAT by hardware and software? According to AM64xx datasheet, and TRM, the Industrial Subsystem supports MII and RGMII by hardware. Also the PHY which is used in AM64 EVM does support both…
Hi Rajat,
I overtook this issue from Frank. I was able to solve the problem by adapting the paths in imports.mak and installing the compilers manually into the specified directory. The build with makefile is now successful. Thank you very much for your support…
Part Number: AM6421 Hi,
In one of our variant (platform based on AM64xx) we need to have up to 6 SPI slaves per MCSPI channel. Is there any hardware limitation for MCSPI to use 6 slaves per channel? I have seen 4 CS per MCSPI. Does that mean a single MCSPI…
Part Number: AM6421 Hi,
Is it possible to access all the peripherals in the isolated core (M4F) from real time (R5F) or application core when not configured in non isolated mode
Thank you