Part Number: AMC0311R-Q1 Hi Team
Now we develop a OBC product, and we use the AMC0311R-Q1 to detect the voltage of the High voltage Bat. From the datasheet , i get that the Nonlinearity of VINP = 0.25V to 2.25V is 0.08% max.
But it is not the max…
Part Number: AMC0311R-Q1 Dear TI experts,
My customer made their schematic using AMC0311RQDWVRQ1. Could you review this schematic?
+HV = 1000V
Applied 5V full scale. Customer will use the range 0V ~ 4.5V.
Best regards,
Chase
Part Number: AMC0311R-Q1 Other Parts Discussed in Thread: AMC0311R Hello,
For AMC0311R-Q1 the recommeded conditions are given as -
But the absolute max ratings are as below -
So as per above absolute limit of upto 7V, can I apply 4.81V to the…
Part Number: AMC0311R-Q1 Other Parts Discussed in Thread: AMC0311R , TLV9001 , AMC0311D , AMC0311S , ISOTMP35R
Hello,
In AMC0311R-Q1 datasheet, the clipping voltage = Nominal analog input voltage.
But, as per below equation on page 20 of datasheet…
Part Number: AMC0311R-Q1 Other Parts Discussed in Thread: AMC1311 Hi team,
My customer is evaluating the impact to isolated sensing secondary supply overvoltage because of the power IC failure. Could you please kindly help suggest the expected device…
Part Number: AMC0311R-Q1 Other Parts Discussed in Thread: AMC0311S , AMC1311 , AMC1351 , AMC0311R Tool/software: Dear team,
My customer wants to measure automotive 12V-Batt voltage with isolated manner because the system is hot-side MCU configuration…
Hello Brian,
To add onto Jiri, I have attached a comparison table with the AMC0311S/R vs ADUM4195 that can hopefully provide some more information on the differences
You are correct, neither device is functionally compatible with each other, **…