Part Number: AMC1100 Dear TI team,
Good evening.
We are measuring AC voltage of 50KHz switching frequency and fundamental frequency of 50Hz at input side of AMC1100,which is very noisy.(Kindly find the attached images of waveform.doc)
We are not getting…
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1200 , Hi,
Could you please tell me that is the difference between AMC1100 and AMC1200? Is there a document to describe the difference?
Thanks.
Kevin Xiong
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1200 Hi team,
I have one question about surge immunity test of AMC1200 and AMC1100.
on AMC1200 datasheet Viosm is 6kV.
and for AMC1100 Viosm is 4615V. but Vtest is 6kV.
1, these Viosm means…
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1200 , AMC1302
Team,
Assuming SOIC (DWV) | 8 package: Are the below options P2P dropped-in replacement to AMC1100?
AMC1100 vs AMC1200 vs AMC1200-Q1 vs AMC1300 vs AMC1300B-Q1 vs AMC1302-Q1
Since…
Part Number: AMC1100 Other Parts Discussed in Thread: ADS1234 , XTR105 , ISO124 , RCV420 , , ISO224 , AMC1336 , ADS131M04 , ADS131A04 , ADS131E04 , REF70 , REF7025 Dear Sir/Madam,
We have below specification from client to sense Analog inputs. We are planning to…
Hi Tom,
I answer here on behalf of my colleague Erol. This is our current circuit.
- On a first stage we attenuate the AC voltage down to the +-250mV analog input range of the AMC1100.
- On a second stage we convert the +-2V analog differential output…
Part Number: AMC1100 Hello Guys,
Good day.
Our customer have built-up a PCB design using AMC1100. The unit is perfectly linear for a portion of input voltages and then at a certain point it goes non-linear. They made sure to follow the design guidelines…
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1300 , AMC1200 Hi,
I am using AMC1100 with a zener diode structure, datasheet fig. 39, to provide 5V for the High Side. The aim was to supply 5V to AMC1100 directy from input voltage, without using…
Part Number: AMC1100 Other Parts Discussed in Thread: TINA-TI , AMC1311 Hi
While simulating AMC1100 part on TINA software for controlling my input current following things were observed.
Without AMC1100 part connected, on controlling the ON/OFF of the…
Part Number: AMC1100 Hi,
I'm using AMC1100 analog isolator for current sensing application.
input side of the amplifier is connected between 5V and ground_1 and output side is connected between 3.3V and ground_2.
there is a voltage difference between…