Part Number: AMC1100 Other Parts Discussed in Thread: AMC1300
Hi,
We are trying to design an isolated amplifier for AC voltage measurement. AMC1100 outputs a differential voltage proportional to the input differential voltage.
But the ADC used along…
Part Number: AMC1100 Hi,
My customer is having issue for the AMC1100, it will have issue of 10MHz to 11MHz EMI comes from the device, may I ask how to filter it?
Great thanks for your help.
Please refer to the capture from the schematic, and let me…
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1300 , Hello, I would like to know if I reverse the phase and the neutral line will this circuit still work? Best regards Haris
Part Number: AMC1100 Other Parts Discussed in Thread: ADS1115 Hi Team,
I am using AMC1100 for a current and voltage sensing application. I just hooked up a simple circuit on breadboard in which high voltage side of AMC is used for measuring voltage for…
Hi Kai,
Input Voltage across VDC+ and VDC- is measured and compared with the voltage across RA0 and RA1 multiplied by gain.
No additional circuitry or differential amplifier is used at the output of AMC1100.
Regards,
Muthu S
Part Number: CD4066B Other Parts Discussed in Thread: AMC1100 , , TMUX1511 , CD4016B Hi,
I am using CD4066B analog mux IC in series with AMC1100 as shown in the attached picture.
My requirement is to switch a resistor that can control the current in the…
Part Number: AMC1100 We have an application with thermocouple and AD8495 and buffer on isolated side. With no probe, AMC1100 sees 1.5V differential with pin 3 on floating ground.
We expect fully saturated positive output, but occasionally see fully saturated…
Part Number: AMC1100 Other Parts Discussed in Thread: AMC1336 , AMC1303E0510 Hi,
A customer wants to use AMC1100 to measure current and voltage on several 230V~ lines and needs 2.5kV isolation. Because of the multitude of measurment paths current consumption…