Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 Hello TI Team,
I am planning to AMC1200-Q1 for AC Voltage Sense. Does AMC1200-Q1 support for AC voltage Sense?
If yes then,
Can you explore me the point VINN and GND1 is short?
or please…
Part Number: AMC1200 Hello , I am planning to use AMC1200 in voltage measurement , there are going to be 2 different ranges 1000Vpeak range and 100Vpeak range.
A relay is used to switch voltage divider branches in order to switch between ranges.
The schematic…
Part Number: AMC1200 Other Parts Discussed in Thread: TMS320F28379D , , AMC1311 I am using AMC1200 to sense the voltage. I need to connect with a C2000 TMS320f28379D and need to apply proper scaling to measure the voltage. Kindly advise me on how to scale…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC3330 , AMC1311 Hello TI Team,
I am planning to use this part :AMC1200BDWV for DC voltage sense.
As per datasheet,
The VIN is shorted with GND1 why?
what are the advantages and disadvantages…
Part Number: AMC1200 Other Parts Discussed in Thread: TIDA-00555 , , AMC1100 , AMC3330 Hello ,
I have been studying the voltage measurement techniques using AMC1100 and AMC1200 as in TIDA-00555.
I have two questions regarding the design.
First , what is the…
Part Number: AMC1200-Q1 Other Parts Discussed in Thread: AMC1200 , AMC3301 Hello,
I am using AMC1200-Q1 for isolated voltage sensing.
The sense resistor across AMC1200-Q1 is 673 ohm & max drop across it is 246mV.
But, the current through it is 375uA…
Part Number: AMC1200
Hi,
I'm facing issue related to noise and voltage hunting at AMC1200 and OP-AMP output.
Please check the schematic if any thing is wrongly connected.
R20-2Mohm,R22-2Mohm and R24-1Kohm
C20-10nF,C22-0.1uF,C24-0.1uF
R342,R346…
Hi Amr,
what sort of overvoltage are we talking about? If it's only ESD, then you can easily add them, although the AMC1200 already contains ESD protection diodes at the inputs.
But if the overvoltage condition lasts longer than ESD, you will need…
Part Number: TPS565201 Other Parts Discussed in Thread: AMC1200 , , TPS561208
Hello ,
I am using AMC1200SDUBR as an isolation amplifier in a voltage measurement PCB. I have a large quantity of the boards and they are behaving in a similar manner.
In order…
Part Number: AMC1200 Hi Team,
My customer is using AMC1200 to monitor the voltage of battery pack (400V). About the input anti-aliasing RC filter, we found some interesting things as bellow:
1) Figure A, with RC filter (10ohm, 330pF), the sampling result…