Part Number: AMC1204 Hi guys, I am taking a look to SBAA094 and I don't understand behavior of sinc filter on VHDL code about input bitstream:
- ...000000... means -Vref - ...111111... means +Vref - ...0101010 ... means 0V
At reset DELTA1 is set to…
Part Number: AMC1204 hi,
i want to use this ic,but i am getting to which controller pins i need to connect clock and data pins. i am using MKE16Z32VLF4 controller.
Part Number: AMC1204 Other Parts Discussed in Thread: AMC1210 Hi Expert,
The customer is surveying the AMC1204 into the AC charging station applicant.
And they will use the MCU,STM32F407 to read it.
Pls advice how to read the AMC1204 output signal…
Part Number: AMC1204 Hi all,
we are using the AMC1204 Sigma Delta modulators. Its output goes into a CPLD where we have implemented a sinc3 filter based on the application note SBAA094, because we have observed some unexpected values, in particular…
Hi there!
Welcome to our e2e Forum!
This is actually an MSP430 question, but let's get some more information on how you are implementing the signals to the AMC1204. For your SMCLK - the sinusoidal nature of the first capture above could be due to…
Hello Vahe,
Thanks for your post and welcome to the forum!
The AMC1204 is an isolated modulator which means that it will produce a bitstream of 1's and 0's proportional to the input signal applied to the high side of the device. This bitstream is…
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1204 , Dear Teams,
According to datasheet, the Vcm for AMC1306M25 (0.16 to AVDD-2.1V) is narrow than AMC1204's Vcm (-0.16 to AVDD). Also, the CMRR for AMC1306 95db is smaller than AMC1204's…
Part Number: AMC1306M05 Other Parts Discussed in Thread: AMC1204 Dear Teams,
My customer is asking the difference between AMC1306 and AMC1204 based on AMC1306's m anchester coding feature. Based on what I know so far, AMC1306 with manchester coding…
Hi Denesh,
We have the EVM board available for this device on the product folder. Can you use that for your evaluation? If not, I would recommending posting a question on the following forum. The experts on these products will be able to guide you better…
Part Number: AMC1204 Dear Team,
The TIC pin define on French LINKY electricity meter is V+ power , Ground and TX .
The data signal is only 1 pin TX output but AMC1204 input is differential input ( IN+ , IN- ) .
How do we connect TX data to AMC1204…