Part Number: AMC1204 Dear Team,
The TIC pin define on French LINKY electricity meter is V+ power , Ground and TX .
The data signal is only 1 pin TX output but AMC1204 input is differential input ( IN+ , IN- ) .
How do we connect TX data to AMC1204…
Part Number: AMC1204 Hi team,
My customer is using AMC1204B for motor drive application.
I'd like to know if the primary side power is off(AVDD), meanwhile secondary side DVDD and CLK signal are good, what is the expected output signal? Is it H or…
Part Number: AMC1204 Hi team,
My customer is using AD7401 from ADI and AMC1204B for performance comparison in below SCH:
However, when using AMC1204B, the error is large(>10%), while ADI part is small. Below data is captured for your reference.…
Part Number: AMC1204 Hello,
To verify my measurement results and unterstand the bandwidth limitations of your modulator and my filter, I want to simulate the modulator as perfect as possible.
Therefore I would need the two integrator time constants…
Part Number: AMC1204 Hi Sirs,
We have done an application for PDM signal generator with AMC1204 EVB.
In this case, we need to translate an audio signal into PDM signal to simulate a DMIC output.
But since AMC1204 was not a recent product, we are…
Part Number: AMC1204-Q1 Other Parts Discussed in Thread: AMC1204 Hello Del-Sig ADC team,
Current systems using AMC1204 with Sinc filters in ASIC. In this case, are the effective bits of the whole system used to calculate by the fomula (K * log (2) M…
Other Parts Discussed in Thread: AMC1204 Hi team,
The datasheet says the chip's 250mv~320mv performance isn't good. (non-linear)
Can we provide the graph to show the performance?
Thank you.
BR
Frank
Part Number: TMS320F28377S Other Parts Discussed in Thread: AMC1204 , CONTROLSUITE I'm trying to work on using a Sigma Delta Filter Module to measure an isolated voltage. From a high level, I would like to read a voltage at 500 Hz.
My hardware is a…
Hi electronicjohn,
Technically, the AMC1204 is a delta-sigma modulator, so its not a complete ADC. It's basically the analog front end of a normal delta-sigma ADC without the filter. The AMC1204 provides a digital bit stream output and allows you to…