Part Number: AMC1210MB-EVM Other Parts Discussed in Thread: AMC1210 Hello,
I'm working on a project with the AMC1210 . At the input from the AMC1210 , I apply the MDAT signal from the ADuM7701 becuase this is similar to AMC1203 function (MDAT).
The voltage…
Dear Tom,
Thanks for reply.
Please suggest a microcontroller which can
support Manchester decoding. Please also let me know, does AMC1210 supports Manchester decoding with 16 bit resolution?
Thanks and Regards,
Raju Baddipadige
Part Number: AMC1210 Other Parts Discussed in Thread: AMC1035 Hello,
We are using AMC1210 with AMC1035 and connected to filter 0 of sinc filter.
Configuration register values are:
#define AMC1210_CONTROLPARAM_FLT0_CFGVAL (0x0000u)
#define AMC121…
Part Number: AMC1210 Dear Team,
we want to use the AMC1210 device in our System.
1) We have some questions on teh RST/ Signal of the device:
- does the signal only connect to Interrupt Module (as shown in block diagram) or to the complete control Module…
Part Number: AMC1210 Dear Team,
we would like to use AMC1210 for decoding of the DS-datastreams, but we will not use the signal generator of the device.
Can we operate the device w/o 5V suppy in the AVDD rail?
Thanks! - Joe
Hi Alex,
Sorry for the long delay.
I won't be able to provide a schematic, however I can let you know that the signal on the CLK line of the AMC1210 is supplied by a 32 MHz clock oscillator chip.
The register values I gave to you initially were confirmed…
Part Number: AMC1210 Other Parts Discussed in Thread: AMC1204 I am using AMC1210 & AMC1204 for precision data conversion.
All the four channels of AMC1210 is connected to independent AMC1204
My register values are as below
Control register - 0x80…
Part Number: AMC1210 Other Parts Discussed in Thread: AMC1204 Hi, all
What is the SH1 and SH2 pins of AMC1210? How to work?
Can I connect without anything?