Part Number: AMC1302 Other Parts Discussed in Thread: AMC1350 , AMC1311 Hi,
I am trying to use AMC1302 to measure the voltage. The schematic is shown here. VDD1 and GND1 are connected with a 5V voltage supply. VINP and VINN are connected with the power…
Part Number: AMC1302 Other Parts Discussed in Thread: AMC1203 Hi Team,
My customer is evaluating AMC1302 with Tina simulation file below,
IL_sensor circuit_use AMC1302.TSC
there are some questions below from customer,
1. VM1 and VM2 are AMC1203 input and…
Part Number: AMC1302 Hello,
We are investigating using the AMC1302. There is a 1µs to 1.5µs delay between an input step reaching 50% of full scale and the output voltage rising to 10% of full scale.
Is this purely due to the amplifiers in…
Part Number: AMC1302 Hi Team,
Hope you are doing well!
I found AMC1302 and AMC1303 have difference in the output format. AMC1302 will output analog signal while AMC1303 will output digital signal.
1. What is the application about those two device?
2.…
Part Number: AMC1302 Hello,
I am trying to implement a AC current sensor which has a variable frequency and can reach up to 250 KHz (shunt resistor is on the HIGH side). For that I am using AMC1302 as an isolation amplifier followed by a differential…
Part Number: AMC1302 Dear TI,
I am going to buid an inverter prototype with 1500V DC-link voltage. The output voltage is 690V (L-L rms). I am wondering if AMC1302 can be used to measure the current or voltage in this situation? I see in the datasheet…
Part Number: AMC1302-Q1 Hello guys,
One of my customers uses AMC1302-Q1 for their current products. At this moment, they need VDE/UL certification documents to sell the products to world wide. AMC1302-Q1 datasheet says that the device has been certified…
Part Number: AMC1302 Other Parts Discussed in Thread: PSPICE-FOR-TI , TINA-TI Hello,
There is any way to include the model of AMC1302 to simulate it on PSPICE-FOR-TI? I have seen the 1301 but some characteristics are differents and I'm looking to simulate…
Part Number: AMC1302 Other Parts Discussed in Thread: AMC3302 Hi,
What is the maximum voltage of HV+ that can be used, when using AMC1302 in phase current measurement for BLDC motor current sensing application.
Can we use 20Khz PWM switching.
regards …