Part Number: AMC1303M2520 Hi, Team.
I've been asked by customer how Method B1 test screes "contamination" out by taking place Method B1 Partial discharge test?
I know that Method B1 is composed of 2 different purpose test , 1 is for HV withstand…
Hello again.
So is there any information on this?
To make it clear i'm providing two pictures, showing what MCU needs to get, and what AMC gives to the MCU. On the first picture it's seen, that SD filter of the MCU needs data to be stable on the rising…
Hi Li Xiang,
I'll get a resolution for the apparent mis-match in the text versus the diagram in the AMC1303M2520 datasheet. There is no 'start or stop' bit associated with these devices, it's just a continuous data stream. If the AVDD supply is missing…
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1303M2520 , , TMS320F28377S
Customer did a performance test with AMC1303M2520/AMC13032510 and AMC1306M25. They found the AMC1306 coming with noise problem on sampling wavefrom. We would like…
Part Number: AMC1303M2520
Hi Arek,
Could you help provide the clock variety distribution of the AMC1303M2520 at room temperature(at 25 degree)?
After I checked with datasheet, I only found out 19.2 ~ 20.8MHz(4% tolerance) for full temperature(-40…
Part Number: AMC1203 Other Parts Discussed in Thread: AMC1210 , , AMC1303M2520 My analog input signal is a positive voltage from a single-ended source. How should I configure the AMC1203 to accept this input, rather than a balanced input?
Hello Yichi,
I am Minkyun Noh, working with Kiron on a project using LMG5200. I have a follow-up questions on your last answer.
1. It seems that 0.5 A is the current 'needed' to charge Qcb = 25 nC for tmin = 50ns. Can we say this is the maximum current…
Part Number: AMC1306E25 Other Parts Discussed in Thread: AMC1303M2520 , , AMC1303E2520
Hi,
I have a sort of follow up question form: https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/611464?tisearch=e2e-sitesearch&keymatch…
Hi Shih kai shegn,
Take a look at the AMC1303M2520, or the AMC1306M25, these are both rated for 100kV/us typical. As processes evolve, we'll rate CMTI higher.
The Manchester decoding block is broken and sporadically stop working.
I have tried replacing my chips, my MCU, terminating data lines, soldering the Agnd, V+, V- pins together, changing SINC and DOSR, any many other thigs and I was getting the same…