Dear Ramesh,
Thank you for your review.
I have tested the performance of the AMC1306E25 in our test board by executing the same Sigma Delta Initialization routine as in the IDDK_PM_Servo_F2837x.c file and monitored the values of the offset_SDFM1 and offset_SDFM2…
Hi Alberto,
Can you provide a little more detail here? The TIDA-00080 document has both current and voltage sensing options with the AMC1304M25 device. Are you looking for a different voltage sensing device or do you want to change to the AMC1304L05…
Kiss,
Effective resolution (ENOB) not only depends upon SDFM (FilterType, OSR) settings, it also depends upon SD-modulator (order, Sampling frequency of SD-modulator. There are many SD-modulators which support 20MHz sampling frequency.
Please check…
Part Number: TMS320F28377D Other Parts Discussed in Thread: AMC1304M25 hi !
in controlsuit the example project IDDK_PM_Servo_F2837x_v2, when i used the sdfm to sample the motor current, I have some question about the conversion coefficient show in the follow…
Part Number: AMC1305M25-Q1 Other Parts Discussed in Thread: AMC1305M25 , AMC1304M25 Hi,
I am looking for a isolated dc voltage sensing solution with max gain error to be less than 0.2%. One possible chip is AMC1305M25. Function-wise it works fine for me…
Other Parts Discussed in Thread: TMS320F28377D , AMC1304M25 Hi,
I am using AMC1304M25 modulator with Delfino uC TMS320F28377D for measuring the high voltage inverter current and I have following queries.
1) I generated a 10MHz Clock using ePWM peripheral…
Other Parts Discussed in Thread: TMS320F28377S , AMC1304M25 Hi,
I am using delta sigma modulator for current measurements of automotive inverter and we want to transfer the current measurements on CAN-Bus.
To test this functionality, I am using AMC1304M25…
Other Parts Discussed in Thread: AMC1304M25 , AMC1304M05 , TIDA-00209 hi all
I need measure dc voltage from array of solar panels. this voltage is Vmin= 75V and Vmax=125V. I will use the amc1304M25 for this work.
I have read the application note SBAA215,…
Other Parts Discussed in Thread: OPA211 , AMC1304M25 , TMS320F28377D , DAC8564 , LMV7219 Hi,
I've looked at the "TI Design" - TIDA-00080- Shunt-Based AC/DC Current and Voltage Sensing for Smart Grid Applications with Reinforced Isolation
In the…
Other Parts Discussed in Thread: AMC1304M25 , AMC1304M05 , TMS320F28377D Hello there,
We are checking the above isolated current shunt and voltage measurement reference design based on AMC1304M05 and AMC1304M25 and we have the following doubts:
1. The design…