Part Number: AMC1305M25-Q1 Other Parts Discussed in Thread: AMC1305M25 , AMC1304M25 Hi,
I am looking for a isolated dc voltage sensing solution with max gain error to be less than 0.2%. One possible chip is AMC1305M25. Function-wise it works fine for…
Other Parts Discussed in Thread: AMC1305M25 Hi all Would you mind if we ask AMC1305M25? <Terminal processing of NC pins on the datasheet> -1pin : This pin can be connected to AVDD or can be left unconnected -5pin : This pin can be left unconnected or…
Other Parts Discussed in Thread: AMC1305L25 , AMC1305M25 Hi all Would you mind if we ask AMC1305M25 and AMC1305L25? How much are the max and the min vaule of VClipping of AMC1305M25 and AMC1305L25? We guess that you don't define these vaules. If you have…
Buddhika,
Welcome to C2000 family.
AMC1305M25 requires you to provide clock input. You can either use PWM (or) any other clock source. Please refer to simplified schematics provided in AMC1305M25 as reference. You should be able to probe both GPIO16…
Part Number: AMC1305L25-Q1 Other Parts Discussed in Thread: AMC1305M25
Actually, there is an application project where we use TI Chip AMC1305L25-Q1 whose datasheet is attached.
We have a question about pin13 CLKIN that request 5MHz to 20.1MHz for…
Part Number: AMC1106M05 Other Parts Discussed in Thread: AMC1305M05 , AMC1305M25 Hi Team
Let me ask short question
a).Does AMC1106M05 have a Duty cycle clock limitation for external clock?(Ex:+/-10%)
b).The differential input resistance is 4.9…
Part Number: AMC1306M05-Q1 Other Parts Discussed in Thread: AMC1305M25 , AMC1306M05 HI SIR
I am survey the TI parts to replace ADI/AD7401
AMC1306M05-Q1 is sames as ADI/AD7401?
thanks
Part Number: TMS320F28374D Other Parts Discussed in Thread: AMC1305F25 , AMC1305M25 Hi champs,
My customer is using F28374D + AMC1305F25 for current sensing function. Based on the measurement, the data setup time is 8.4 ns when data is 0 (data changes…