Part Number: AMC1306E25 Hi Team,
Customer is asking for is we can provide the verilog simulation model for AMC1306E25 to simulate it's function, can you help to check?
Thanks.
Part Number: AMC1306E25 Other Parts Discussed in Thread: LM3480 , TIDA-00914 Hi Ti ,
In the circuit diagram of TIDA-00914, when the AMC1306 is used for current sensing, an LDO(LM3480) is employed between AVDD and AGND to serve as the power source for the…
Part Number: AMC1306E25 Hi team,
If the input voltage is 9mV, with 250mV input range and sin3 filter. Is it possible to realize 14bit ENOB? I'm asking because in this condition, our customer tested the AMC1306 to be 13 bit(ENOB), which means that the…
Part Number: AMC1306E25 Other Parts Discussed in Thread: AMC1336 , AMC1306M05 Hi there,
I knew the input impedance of AMC1306 is small, so I'm promoting AMC1336 for bus voltage sense. But I would like to confirm the error level of AMC1306. In the evaluation…
Part Number: AMC1306E25 Other Parts Discussed in Thread: AMC1306M25 , AMC1336 I am looking to sense the voltage across a MOSFET in a flyback power converter. I start by stepping the voltage down to about 3V.
Since my input voltage is 300V, I need to then…
Part Number: AMC1306E25 Hi Team,
Can you explain what's the usage of PWMx here in simplified schematic of datasheet? If customer don't have enough resources to connect here, what's influence it will cause?
B&R.
Stanley
Part Number: AMC1306E25 Other Parts Discussed in Thread: C2000WARE Tool/software: Code Composer Studio Hi friends
I am using AMC1306E25 module to read the 4 voltages with a switching frequency of ~ 250kHz in drive application. As this is manchester coded…
Part Number: TMS320F28377D Other Parts Discussed in Thread: AMC1306E25 , CONTROLSUITE Hello I'm Moonhyun.
I'm working on in-house control board with 28377D and trying to use SDFM module with Manchester decoding function (mode 2).
The application…
Part Number: AMC1306E25 Other Parts Discussed in Thread: AMC1303M2520 , , AMC1303E2520
Hi,
I have a sort of follow up question form: https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/611464?tisearch=e2e-sitesearch&keymatch=%20user…
Part Number: TMS320F28375S Other Parts Discussed in Thread: AMC1303E2520 , AMC1306E25 , AMC1303M2520 Hi,
I have a 3 phase PFC application. I measure 3 phase currents, 3 phase voltages, dc voltage and dc current. The 3 phase voltages are "smooth" 50Hz, the…