Part Number: TMS320F280049C Other Parts Discussed in Thread: AMC1306EVM , C2000WARE Hi
I try to use AMC1306EVM to test SDFM program. I made some changes on file sdfm_ex4_pwm_sync_cpuread.c
under folder //ti/c2000/C2000Ware_3_02_00_00/drivelib/f28004x…
Hi Jaikai,
Glad that you found the issue. Request you to mark the relevant answer as 'Resolved'.
For the query on AMC1306EVM, I would recommend you to refer AMC1306 Reference Guide . Section 4.3 explains on the pin details to use as input for clock…
Hi Jiakai,
The AMC1306M25 comes in a DWV00008A package, not SOIC-8. The details can be seen here: https://www.ti.com/lit/ml/mpds382b/mpds382b.pdf
or at the end of the datasheet. I recommend purchasing an evaluation module (EVM) to assist with your…
Part Number: AMC1306E25 Hi Expert,
Customer is test AMC1306E25EVM and below is setup.They find there is a 0.14mV offset when external short J1. When input 256mV, device output 199mV results. Could you give a troubleshooting steps to find the root…
Part Number: TIDA-00080 Other Parts Discussed in Thread: AMC1306EVM , C2000WARE , CDCE906 , AMC1306M25
Good morning.
I was wondering if I can get some advice about the problem I meet with.
The final goal is to operate the TIDA-00080 reference design…
Hi Manoj,
sorry for the late reply...I took this topic over from Sandesh and we could resolve all our problems with the sigma delta modulator excpect the wrong sign of the measurement data. To make sure that we have no HW problem in our design, we purchased…
Dear Sam,
thank you for your interest in TIDA-00915 and current/voltage sensing. The TIDA-00915 GaN inverter is rated for 200-400V DC-link voltage and the LMG3411 are isolated from the C2000 controlCARD. An inline shunt requires an isolated amplifier…
Hello Yuyama-san,
Please see attached. Please not that not much was changed, Rev B is to incorporate the AMC1336 device revision on the same board. sbau271.pdf