Part Number: AMC1306M25 The application scenario is current sampling driven by motor servo,This is the diagram:
Encountered two problems:
There are burrs in the current sampled by the software when the motor is idling。
The sampling current…
Part Number: AMC1306M25 In the d/s, it specifies that the AVDD high side supply voltage is between 3V to 5.5V. yes, we know it's defined on the d/s. however Customer would like to know what is the min. operating voltage that doesn't specify in d/s? is…
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1306M05 Tool/software: hi
I want to know the DC accuracy parameter from -250mV to -320mV and 250mV to 320mV for a worst Case Calculation, could you provid it? thank you!
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1306M05 there is some error at the current sensor data. like 0.25A dynamic error.
AVDD is 5V, about 50mV voltage ripple.
does this affect sample accuracy? how much it will impact.
Part Number: AMC1306M25 Hi team,
I would like to know if the high and low CLKIN voltage are reasonable, as long as they meet the range in the following figure?
Thanks!
Regards,
Ivy
Part Number: AMC1306M25 Hi expert,
Customer is seeing our AMC1306M25. Due to AMC1306's AVDD power is not that stable in real products, for the figure 53, under what voltage for AVDD will trigger fail-safe mode? And what's the time delay for missing…
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1350 , Hi team,
Customer wants to know whether the offset error can have aging degradation. They need to know the offset error(+/-100uV min/max) can be increased in two or three times by…
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1305M25 , Hi,
in the datasheet of AMC1305M25 section 7.10 is shown Vclipping with 312.5mV Typ.
For AMC1306M25 it is shown with 320mV.
Are both values correct, if yes what's the reason…
Part Number: AMC1306M25 Hi,
What is the UL number of AMC1306M25DWVR? Is it number for UL-US-L181974-14-02604102-3 on the attached file?
Please help to confirm, thanks~
sbaq007-amc1306.pdf
Part Number: AMC1306M25 Hi team,
What is the flammability rating of AMC1306M25? I didn’t find it in the datasheet. Do you have related materials?
Really appreciate your help!
Thanks & Best regards,
Wendy