Part Number: AMC1306M25 Hi Experts:
I have one question regarding the resistor on the digital output , my customer add the resistor in series in the CLK and DOUT trace and found the value of the resistor
have big impact on the data reading.
If they…
Part Number: AMC1306M25 Hello~
I have three questions.
Question 1. -> When a single clock is generated by the MCU, The AMC1306 is output in bitstream form via the DOUT pin.
Is it correct to receive 1 bit from the MCU as a digital input?
If not…
Part Number: AMC1306M25 Hi team,
Customer has concerns about the behavior of digital output of AMC1306M25 when the input voltage value exceeds the specified linear range.
The datasheet mentions at 8.3.4 Digital Output that the output of the modular…
Part Number: AMC1306M25 Hi Experts,
We want to know how to estimate below.
Detection error
Temperature drift
We are assuming that we can get them by using Gain Error(E_G), Gain Error thermal drift(TCE_G), Offset Error(E_O) and Offset Error…
Part Number: AMC1306M25 Hi team,
I am helping my customer survey C2000+ sigma delta modulator in their next gen platform.
The main concern is about the delay of AMC1306. In order to achieve 12bit resolution, they need to run AMC1306 in Sinc3 mode…
Hello Scott,
Thanks, that's helped me to fully understand the Fail-safe output on DOUT.
I would suggest that the description of the Test Pattern being alternating 1's and 0's are added to the next update of the datasheet to avoid any ambiguity regarding…
Part Number: AMC1306M25 Hi all Would you mind if we ask AMC1306M25? <Question1> In case of input range between ±250mV and ±320mV, how much will the output data code? On the datasheet, there is the description; "A differential input of 250 mV (for the…
Part Number: AMC1306M25
Regarding to the SNR performance for AMC1303, AMC1306 and AMC1305, why they are differences with temp and Vin change?Is this because the process difference or others?
Regards,
Brian
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1204 Hello team,
Hope you are well. When you get a chance please see below customer question:
We need the PWM clock frequency to be adjustable in the 20 to 200 kHz range (as opposed to a…
Hi Fearghal,
For the AMC1306M25, you are correct, the modulator has more setup and hold time against the falling CLKIN, which is not the edge that the DSP is using. You could use an inverter to capture the clock from the PWM output to the SD_Dx input…