Part Number: AMC6821 Hi team
AMC6821 has a rating for the operating temperature range and absolute maximum junction temperature in the datasheet, but no info on recommended value for these.
My understanding is that the device will instantly malfunction…
Part Number: AMC6821 Hi TI expert,
We encounter similar issue as below.
After checking the below link that it mentioned we can use 9 CLK to recover the I2C bus and the Configuration Register 4 bit 7 description.
AMC6821 Reset I2C Hanging the Bus by Holding…
Part Number: AMC6821 Dear Team,
There is a good news that we have a chance to replace ADT7475.
Could you help to share the detailed comparison table ( ADT7475 vs AMC6821) for me? We appreciated your great support!
Many Thanks,
Jimmy
.
Part Number: AMC6821 Hi,
I have doubt in regarding AMC6821 application
1) can we connect 24V fan to AMC6821 2)If we have any application circuits for 24V fan , share those files.
Regards,
Srinivas
Hi Renan,
Sorry for the delay here, but I now have the thermal characteristics for the AMC6821-Q1.
Thermal Metric
SSOP-16
UNIT
R ΘJA
Junction-to-ambient thermal resistance
102.3
°C/W
R ΘJC(top)
Junction-to-case (top) thermal…
Part Number: AMC6821-Q1 Other Parts Discussed in Thread: AMC6821 Hi team,
I would like to confirm with you one question below.
How to connect IN+/IN- if we do not need remote temperature sensing?
Thanks.
Johnny
Part Number: AMC6821-Q1 Other Parts Discussed in Thread: AMC6821 Hello. I use amc6821 for MCU fan control.
For chip init, I call amc6821 reset & initializing function.
After i2c init and 50ms, I call amc6821 reset & init function, and I cannot control…
Part Number: AMC6821 Hi, I have a few questions on the pins of the AMC6821.
1. TACH pin: does the AMC6821 read the fan speed through the sensor pin of the fan connector? I.e a 4 wire fan connector that has 12V, GND, PWM, and Sensor, where the TACH pin…
Part Number: AMC6821 I’m importing the schematic symbol and footprint from the TI website and I can see the schematic symbol fine (first image), but the footprint isn’t showing. (.PcbLib file second pic ) Have you ran into this, and been able…
Part Number: AMC6821 Hey team,
I was curious how the AMC6821 prioritizes addressing temperature if there is a difference between the internal temperature of the device and the temperature it is reading from its 'substrate sensing transistor'
…