Part Number: LM96080 Other Parts Discussed in Thread: AMC80 , Tool/software: I need a LM96080CIMT/NOPB part , junction to board resistance and Junction to Case resistance (Thermal Data)
Part Number: LM96063 Other Parts Discussed in Thread: AMC80 , LM96080 , LM96194 , LM94 , LM96000 , LM93 Hi,
We currently have a project for the Intel Q670 platform. We have a total of 4 fans (2x SMART FAN and 2x non-Smart 12V FAN). However, due to the…
Hi Diego,
The tio32.ini file needs to be moved into the "data" folder in the software installation folder.
Please navigate to C:\Program Files (x86)\AMC80 and move tio32.ini into the data folder, as indicated below.
We will work on pushing this…
Hello MINGKUN HE, Thank you very much for reaching out, the values suggested in the LM96080 datasheet are selected such that the resistance values are " low enough to avoid errors due to input leakage currents yet high enough to protect both the inputs…
Hi Bonnie,
TMP512, TMP513 Local + 2/3 Remote Temperature and Digital Current Shunt Monitor
ADS1118 16 bit, 4 channel ADC with Local Temperature
Several devices under "Monitoring and Fan Control" such as AMC80 have Local Temperature + ADC + Fan PWM…
Other Parts Discussed in Thread: AMC80 Hi
AMC80 Datasheet(SBOU101) page20 Figure26 AMC80EVM-schamtic
A schematic(Picture) blurs.
The resistance-value and capacitance-value can't be understood from a schematic(picture).
Please provide the connection…
Kuan,
We don't have a single device that will fit all of your requirements so you might have to use more than one device. Here is the list. It looks like you might want to consider these: LM96194,LM94,LM93,LM96000.
HW_Fan_Parametric Search.xlsx
…