Part Number: ARM-CGT When I use a library like 'ipc.lib' which includes 'a.obj' and 'b.obj', how can I put the '.text' section of 'a.obj' to a group like 'mygroup'.
Furthermore how can I just put a function…
Part Number: ARM-CGT description
1.I use "-m project.map" to generate the map file, but some variable don't have memory address information,such as Rte_InitState
2.Then I use " --mapfile_contents=all \ -m project.map " to generate…
I apologize for the delay.
Thank you for submitting a preprocessed file. With that, and some help from Marie H, I am able to reproduce the same behavior. I filed the issue EXT_EP-11012 to have this investigated. You are welcome to follow it with that link…
Part Number: ARM-CGT Other Parts Discussed in Thread: SEGGER Is it possible to use the ARM-CGT tools for compilation/build and use GDB to debug?
Thanks!
Part Number: ARM-CGT
Hi,
is there any compiler errata sheet available for the different versions of TI ARM CGT? We would need that in a certification process to show in our certification process, that we are not running in a compiler bug.
Best regar…
Part Number: ARM-CGT I'm working on a project that is using Code Composer Studio v5 for compiling our DSP. This is running on a Windows XP virtual machine.
I would like to get a more contemporary compiler to produce identical object code.
Is there…
Part Number: ARM-CGT I am combing two elf file using the armhex tool but I am now seeing this error:
armhex --load_image --load_image:format=elf --load_image:endian=big --load_image:combine_sections=true bootloader.elf application.elf -o app.elf
error…
Part Number: ARM-CGT Other Parts Discussed in Thread: HALCOGEN Currently we using ARM-CGT-XX, and considering if moving to ARM-CGT-CLANG-X is an option.
Is that version supported for all the TMS HalCoGen HAL layers, and does ARM-CGT-CLANG-X allow for application…
Ali Ghadyali said: On thIs compiler the code generates a message shown above and crashes the program.
Can you clarify how the program crashes?
While there is EXT_EP-9743 on the subject of the warning (remark #342-D) the existing bug doesn't seem to mention…