Part Number: AUDIO-AM62D-EVM Tool/software: Hi,
I need to create a static .lib library for C7000 of AM62d but i can't.
I imported the empty project and i can't change the project output type in CCS.
Please Advice
Hi Senthilkumar,
senthilkumar N said: Have you tried capturing the UART logs in C7x? I need those specific logs, not the CCS logs.
I couldn't fully understand your query. The image I sent earlier is c7x log only, just it is displayed through the CCS…
Part Number: AM62D-Q1 Other Parts Discussed in Thread: AUDIO-AM62D-EVM
Hi TI experts,
I am planning to reuse the AM62D-Q1 AUDIO-AM62D-EVM schematics for my custom board design. I see the below schematic sections (pages) added to the AUDIO-AM62D-EVM…
Kaviyarasan Balakrishnan said: , but I am unable to build the C75 and MCU-R5F projects.
Please check the properties of this project.
Right click on the project and open properties. Navigate General -> Dependencies.
Part Number: AUDIO-AM62D-EVM Hello,
which SDK can I use with the AUDIO-AM62D-EVM which supports Linux.
I see AM62X SDK does not support AM62D. On TI.com AM62D only has the AudioWeaver SDK - Is that Linux or FreeRTOS based?
And can AM62A SDK be used…
Part Number: AUDIO-AM62D-EVM Other Parts Discussed in Thread: SYSCONFIG Tool/software: I am currently using Code Composer Studio (CCS) v20.2, but I’m still facing an import issue when working with SDK 11. Despite having tried with this CCS version, the…
Part Number: AUDIO-AM62D-EVM Tool/software: Hi AM62D Team, I tried to enable NOR boot from AM62D-EVM Board, I am able to build the image but it does not work. the short power up log is:
U-Boot SPL 2025.01-00485-g74e16c1e4b41 (June 26 2025 -16:22:47…
Part Number: AUDIO-AM62D-EVM Tool/software: Hi experts,
When developing a USB driver for the AM62D, could you please tell me the steps, such as how to obtain the necessary documentation? Or, can I use the same specifications that I obtained when developing…
Hi James,
Thank you for your reply.
JJD said: How are you measuring performance? Can you post logs?
Please refer to the thread below for information on how to measure performance. (+) AUDIO-AM62D-EVM: Difference in execution clock cycles between…
Part Number: AUDIO-AM62D-EVM
Tool/software:
when developing audio over mcasp0, getting audio slots missing on TX direction but RX direction is good. when transmitting 4 channel audio, only seeing two channel audio out. aplay -D hw:0,0 -c 4 -f S24_LE…