Part Number: AWR1843BOOST Other Parts Discussed in Thread: UNIFLASH Hello TI,
Currently, I am working with AWR1843BOOST EVM and I am completely new to this topic. Regarding the project, We are working on robotic arm and needs to detect the movement…
Part Number: IWR1642BOOST Tool/software: Code Composer Studio IWR1642BOOST DEMO added a serial output function, output an array of data, but the program will run out of error. Below is a screenshot, how is this going?
Other Parts Discussed in Thread: AWR2243BOOST Regarding the AWR2243Boost Evaluation board, the Stuck up layer which was embedded in the design file version A and B shows the Inner layers’ material is FR4- 370H.
While based on the application note (…
Part Number: IWR1642BOOST I'm trying to understand the meaning of the code in the dss_data_path.c.
I think the obj->radarCube stores all the data after 1D FFT.I divide the data in obj - > radarcube into eight parts, corresponding to four RX and two…
Part Number: MMWAVE-STUDIO Other Parts Discussed in Thread: AWR1642
I generated the JOSN configuration file of millimeter wave radar through mmWaveSensingEstimato. I hope to load this configuration file directly through mmWave Configuration File in…
Part Number: AWR1642 As per the old thread of November 2017,
TI was in the process to add support of Ethernet, will you please mention the date of release for the same.
Thanks,
So just to be clear, If I want to run small programs/ algorithms, they can be designed for the DSP in the 1642, or using the Hardware accelerator in the 1443. However, for more complex and heavy computation it is recommend to use DCA1000 to…
Part Number: IWR1642BOOST Other Parts Discussed in Thread: IWR1642 , IWR1443 , IWR6843 Tool/software: Code Composer Studio Hello TI engineer, I am testing with IWR1642BOOST DEMO board now, I want to detect the distance of 150m, can I check the parameter…
Part Number: IWR1642BOOST Other Parts Discussed in Thread: IWR1642 Hi,
In the mmWave Demo Visualizer one of the configurable options is the maximum radial velocity. Based on chirp parameters this appears to be the theoretical max velocity. In the mmWave…