Part Number: AWR1843AOP Tool/software: The general GPIO or communication port side can be processed with internal pull-up or internal pull-down, so it seems that it can be processed as FLOAT when not in use, but
GPADC does not seem to have internal pull…
Part Number: AWR1843AOP Tool/software: Hi all,
We recently tested the AWR1843AOP board in an anechoic chamber and observed constant ghost objects at two ranges: one at 5 m and the other at 140 m.
We were using the MRR lab with a 120 m chirp configuration…
Hi Luca,
Thank you for reaching out again.
It is not recommended that you bypass the SOC_waitBSSPowerUp since bypassing it would indicate that we are no longer validating the state of the BSS before proceeding with the program. Not validating this state…
Part Number: AWR1843AOP Other Parts Discussed in Thread: SYSCONFIG , IWR1843AOP Tool/software: Hi,
By using the AWR1843AOP sensor we want to make an electronics card. In this application there will be a GPIO interface using 2 pins. For this aim we can…
Part Number: AWR1843AOPEVM Other Parts Discussed in Thread: AWR1843AOP Tool/software: Hello. Our team is interested to develop a custom PCB with AWR1843AOP for a university project, instead of directly purchasing the EVM board due to budget constraints…
Part Number: AWR1843AOP Tool/software:
Table 17: Diagnostics Mechanisms Summary: Except for the parts that are specified as System defined, the other items seem to be TI's built-in functions that are automatically operated by hardware or firmware, and…
Hi Jack,
DCA1000 is not meant for production but only for data collection and development.
AWR1843 does not support Ethernet interface.
One option could be using a SPI to Ethernet transceiver PHY and use the SPI interface of AWR1843. But speed would be…
Part Number: AWR1843AOP Other Parts Discussed in Thread: UNIFLASH Tool/software: Playing around with my AWR1843AOP. I'd like to update the demo. code on the board to the 3.6 SDK demo. code so it doesn't complain when using the Visualizer.
Digging…
Part Number: AWR1843AOP Other Parts Discussed in Thread: LP87524J-Q1 , LM60430-Q1 Tool/software: Hi,
I need to check the durability of radar element
Is there a device lifespan time for AWR1843AOP? If you have any information related to durability, please…
Part Number: AWR1843AOP Tool/software: We would like to connect a large flash (1Gbyte) for logging . This flash should support boot as well.
- we are aware that the flash powers up in 3 byte addressing mode
1) will the boot loader work with a large flash…