Part Number: AWR2243
Hello, experts.
I would like to ask about my use of the AWR2243 board. I want to use MMWL_StartFrame() to make the chip start transmitting, and MMWL_sensorStop() to make the chip stop transmitting. However, I would like to know…
Part Number: AWR2243 Hello Ti Support
I have a question, that with Ti AWR2243 is it possible to make it work in the following config:
1) Slave with Rx channels Active only
2) Slave with TX channel Active for TDM mode
3) Master with no active RX…
Part Number: AWR2243 Other Parts Discussed in Thread: MMWAVE-STUDIO , Hi expert,
Can the AWR2243 debug mode be configured using C code? Is mmwave-studio only configurable using LUA scripts?
The customer encountered an issue: when using the AWR2243…
Part Number: AWR2243 Other Parts Discussed in Thread: AWR2188 , Hi all
Would you mind if we ask AWR2243 and AWR2188?
Q1: Are there any differences of middleware between AWR2243 and AWR2188? [Our assumption] We think the basic base is the same, but…
Part Number: AWR2243 Hi expert,
In a four-chip cascaded configuration, after calling the SensorStart function to begin transmission, I attempt to call SensorStop to stop it. However, only the master chip successfully stops. The other chips return an…
Part Number: AWR2243 Hello,
We would like to evaluate whether the AWR2243 can be used for stepped-frequency continuous-wave (SFCW) ranging.
In our intended method, each transmitted signal is a flat, constant-frequency CW tone with no frequency slope…
Part Number: AWR2243 Hello TI expert,
We have developed an AWR2243-based 4-chip cascaded radar and have encountered an issue with TX back-off operation.
As shown in the attached figure, the Tx back-off appears to work properly for the Tx1 and the…
Part Number: AWR2243 Other Parts Discussed in Thread: MMWCAS-RF-EVM Hi TI Support,
I hope you are doing well.
I am a researcher at the University of Glasgow, and we purchased an AWR2243 Cascade Radar System (MMWCAS-RF-EVM) for our research.
The…
Part Number: AWR2243 Other Parts Discussed in Thread: MMWCAS-RF-EVM Hi TI Support,
I am using the **MMWCAS-RF-EVM + MMWCAS-DSP-EVM** cascade radar platform based on **AWR2243**. Since **MMWCAS-RF-EVM** and **MMWCAS-DSP-EVM** cannot be found in the TI…
Part Number: AWR2243-2X-CAS-EVM Other Parts Discussed in Thread: AWR2243 , AWR2243BOOST Hello, I would like to inquire about a few questions regarding the AWR2243-2X-CAS-EVM board card. 1. In the schematic diagram, the two 2243 chips on the circuit board…