Part Number: AWR2944 Hello,
Subject : Enable Cache
1. In ARM Cortex-R Series Programmer Guide - version 1.0 , Link - " ">developer.arm.com/.../System-Control-Register--SCTLR-"
a) In System Control Register (SCTLR) -
"I" bit…
Hello Pradipta,
1. Based on mmwave_mcuplus_sdk_04_06_00_01, I have modified two places:
Open CLI_BYPASS macro and change radar configuration as show in the below image.
Add the below code to MmwDemo_transmitProcessedOutput() interface to reset AWR2944…
Part Number: AWR2944 Hi expert,
Customer want to log the CPU and ESM fault of AWR294x RF. On the ICD of AWR294x, the RL_RF_AE_ESMFAULT_SB message is deprecated and need to use ADV_ESMFAULT.
The ID of AWR_AE_RF_ADV_ESMFAULT_SB is 0x1007.
But in rl_message…
Hi Ivan,
Yes, Rev B has AWR2944 ES1.0 while the latest Rev D has the ES2.0 silicon.
ES1.0 has less memory than ES2.0, and that may cause the demo to fail for larger numbers of objects.
Please show this response to the Customer Service team and request…
Part Number: AWR2944 Other Parts Discussed in Thread: IWR6843 , IWRL6432
Dear TI Support team,
My company specialized in mobility solutions in Europe is looking to design a radar-based device identifying and counting the number of people in pedestrian…
Part Number: AWR2944EVM Other Parts Discussed in Thread: AWR2944 Hi TI Community,
I'm currently working on an experiment using AWR2944 EVM aimed at identifying object distance from the radar and distinguishing between multiple objects while also calculating…
Part Number: AWR2944 Hello Expert,
We set the QSPI input frequency to 80MHz and enabled DMA. Then, I observed the following clock signal waveform(read flash).
CMD
Address
Data
Data
CMD
Address
Data
Data
6BH
A23-A16
A15-A8
A7-A0
dummy
16bytes…
Part Number: AWR2944 Hi,
From the SDK code for AWR2944, we found an function SDL_SOC_controlModuleUnlockMMR, we write the specific value to
LOCK0_KICK0 and LOCK0_KICK1 to do the MMR lock and unlock. Why we have to set the specific value ? I cannot find…