Part Number: AWR2E44PEVM
The following are the steps to calibrate the LOP antenna for the AWR2E44PEVM.
Flash the board with the mmw app image present in the latest SDK.
Example Path: C:\ti\mmwave_mcuplus_sdk_04_07_01_04\mmwave_mcuplus_sdk_04_07_01_04…
Part Number: AWR2E44PEVM I have a requirement that state the following:
1- The Radar SW Shall implement XO/Slicer Frequency Detection circuitry to monitor the REFCLK oscillator output. Note: Safety Manual ID - XOSC_SM2
Questions:
What is the XO…
Part Number: AWR2E44PEVM I have a requirement that state the following:
The Radar SW shall enable boot time LBIST of CPU core and Vectored Interrupt Controller..
Note: - Safety Manual ID - VIM11
Questions:
VIM11 refers to CR4 STC bit in RF_POWERUP_BIST_STATUS_FLAGS…
Part Number: AWR2E44PEVM MCAL_REL_02.02.07.00
Hello,
While integrating this version of MCAL, We noticed that there is a main Function in static code of Cdd_I2c, but there is no Main function period container present in Schema file of the module. …
Part Number: AWR2E44PEVM Hi,
We are working on the configuration of the Aurora TX initialization phase on the TI chip and would like to confirm a few details with you to make sure our settings are correct.
Our current understanding is that the…
Part Number: AWR2E44PEVM Other Parts Discussed in Thread: SYSCONFIG Hello TI,
i am bringing up the SW for AWR2E44P target and i am trying to set the clock source for Ethernet using Sysconfig, i added an instance for Enet(CPSW) and used the default clock…
Part Number: AWR2E44PEVM
Hello,
On the AM62x, we have a direct access mode for the external flash, allowing us to access the stored data directly.
Based on my analysis of the reference manual, it appears that the AWR2E44P does not support this capability…
Part Number: AWR2E44PEVM MCAL version: MCAL_REL_02.02.07.00 Greetings,
In Can_PBcfg.c (line 260), there is a validation check that enforces CanHwFilterMask == 0xFFFFFFFF whenever the CanHandleType of a Hardware Object Handle (HOH) is configured as FULL…
Part Number: AWR2E44PEVM Hello,
MCAL Version : MCAL_REL_02.02.07.00
During integration, we observed that the Fls_MainFunction is blocking, which indicates that there is a loop or wait mechanism that blocks the corresponding caller task.
The FLS…
Part Number: AWR2E44PEVM Other Parts Discussed in Thread: AWR2E44 Based on TI demo pf AWR2E44, we have made the following changes:
The RangeBin is changed to 456;
The input data type of RanCFAR is changed from int16 to uint32;
The CFAR mode of…