Part Number: AWRL1432 I am currently using the awrL1432 EVM, and I have allocated the shared memory from HWASS for APPSS use, and put some code into this section. Normally, if the compiled appImage is burned into flash, it runs fine on power-up. However…
Part Number: AWRL1432 Other Parts Discussed in Thread: AWRL6432 , , AWR1843 , AWR6843 Hello Team,
Our customer has completed development on the AWRL6432 and is now looking to migrate to the AWRL1432 . Could you provide guidance on how to proceed?
…
Part Number: AWRL1432 Currently, our requirement is to use a reset method to jump to SBL within the app. May I ask if it is feasible to directly use SOC_triggerWarmReset or SOC_triggerSoftReset from the SDK? Why does the system crash after directly calling…
Part Number: AWRL1432 Hello Team,
When flashing the AWRL1432 via UART, can the ROM bootloader recognize both UARTA and UARTB ?
The bootloader documentation specifies that both pin pairs—BALL F11/E10 (RS232/UARTB) and J11/L12 (UARTA/UARTB) —are supported…
Part Number: AWRL1432 The driver in the SDK only supports the EPWMA module. I now need to develop the EPWMB module, and it cannot be directly configured in the syscfg file. How should I develop it? In cslr_soc_baseaddress.h, only the address CSL_APP_ETPWM_U_BASE…
Part Number: AWRL1432 I currently have a requirement to pass some parameters between the SBL and the APP, so I need to ensure that when the APP resets back to the SBL, the value of a certain RAM area can be retained, and in the SBL, this RAM area can…
Part Number: AWRL1432 I am currently using the EPWM module of awrL1432 and have encountered the following issues: 1. PWM period is inaccurate. Referring to the epwm_duty_cycle.c file in MMWAVE_L_SDK_05_05_04_02, I modified APP_EPWM_DUTY_CYCLE to 15, APP_EPWM_OUTPUT_FREQ…
Part Number: AWRL1432 Other Parts Discussed in Thread: , IWRL1432 Hello TI Team,
I am evaluating the AWRL1432 radar sensor for automotive short-range radar applications and would like to understand its practical RF performance and supported use cases…
Part Number: AWRL1432 Hi TI experts,
I'm trying to put the AWRL1432 in CW mode. So, I'm using this doc : Enabling Cw Mode Using SDK 5 For Testing.
I flashed the sensor with the motion_and_presence_detection_demo.release.appimage application.
Firstly…
Part Number: AWRL1432 Other Parts Discussed in Thread: AWRL6844 Can the awrL1432 be connected using the v20 version of CCS? You require using SDK_05_05, but I did not find a CCS_SupportFiles folder like in SDK_06_00. Or should I just create a new ccxml…