Part Number: AWRL6844EVM Other Parts Discussed in Thread: AWRL6844 Hello,
This is a following up of my previous thread "AWRL6844EVM: Stability issue with low power mode enable".
The system typically works from 40 minutes and up to 2 hours before the…
Part Number: AWRL6844EVM Other Parts Discussed in Thread: SYSCONFIG Hi TI Support Team,
I encountered an issue where the firmware fails to boot when I select 450 MHz for the DSP core operating frequency via SysConfig.
Investigation: Upon debugging…
Part Number: AWRL6844EVM Hi,
My understanding is that when the device is in the HS-FS state, secure boot is not enforced and debug access to the R5F should be open. However, I am not able to run anything on the R5F. Flashing using arprog_cmdline_6844…
Part Number: AWRL6844EVM Other Parts Discussed in Thread: AWRL6844 Hello Expert,
I am currently working with the AWRL6844 EVM and the DCA1000 capture board, and I need to systematically test all the modes of frame triggering, with a particular focus…
Part Number: AWRL6844EVM Other Parts Discussed in Thread: AWRL6844 Hello TI Support Team,
I am working on implementing SPI-based ADC data logging on the AWR6844EVM following the guide in the mmWave SDK documentation (mmwave_l_sdk_06_00_05_01/docs/api_guide_xwrL684x…
Part Number: AWRL6844EVM Hi expert,
Customer measures the frequcny on SCL of i2c on evm. The speed is 475KHz.
From datasheet, the max speed is 400KHz.
Can you help check this?
BR,
frank
Part Number: AWRL6844EVM Other Parts Discussed in Thread: DCA1000EVM Hello TI team,
I have using mmWaveStudio and SDK 6.0.1 for getting data from a AWRL6844EVM +DCA1000EVM. What I'm doing is retrieved data with the radar covered by a material to avoid…
Part Number: AWRL6844EVM Other Parts Discussed in Thread: AWRL6844 Hello TI Team,
I am reviewing the AWRL6844 CPD (Central Processing Demo) example provided in Radar Toolbox 4.0 , and I have a few questions regarding the DSS/MSS architecture and the…
Part Number: AWRL6844EVM Other Parts Discussed in Thread: AWRL6844 Hi team,
I was wondering does the Awrl6844 new SDK supports an equivalent dynamic chirp configuration API like AWR_DYN_CHIRP_SET_SB in 6243 and 6843?
Best wishes,
Isabel
Part Number: AWRL6844EVM Mcal : mcal-config_03_01_04_00 &mcal-03_01_04_00
Description:
During integration of the MCAL package, a compilation error occurs due to the duplicate definition of the NULL_PTR macro in hal_stdtypes.h and Compiler_Common.h…