Part Number: BOOST-TUSS4470 Hello guys!
I have a BOOST-TUSS4470 + MSP-EXP430F5529LP setup. My goal is to burst pulses using TUSS4470 to excite a transducer in a Pulse-Echo scheme. So it is quite important for me to have control over the excitation pulse…
Part Number: BOOST-TUSS4470 recently we bought it, couldn't find any tutorial for working on it Do you had any sample projects or tutorials for this sensor driver kindly reply ASAP.
Part Number: BOOST-TUSS4470 I'm considering a purchase of the boost-TUSS4470. My primary application is ID Concentration in liquids and solids. Why the recommended transducers only have low frequency? None is represented with 1MHz. Doesn't it require…
Part Number: BOOST-TUSS4470 Hi Team,
Customer would like to know below questions:
BOOST-TUSS4470 is not used with MSP-EXP430F5529LP, but connected with other industrial control boards. Industrial control board is connected with SPI interface and ordinary…
Part Number: TUSS4470
Tool/software: TI C/C++ Compiler
Hello,
Our customer uses MSP-EXP430F5529LP and BOOST-TUSS4470 .REG_USER registers be Setup completed.Next One measurement.
The questions are:
1、How to start a command,command execution flow?If you could…
Part Number: BOOST-TUSS4470 Hello,
Our customer uses MSP-EXP430F5529LP and BOOST-TUSS4470 with SPI communication. The initial code is as following:
//Clock Polarity: The inactive state is high
//MSB First, 8-bit, Master, 3-pin mode, Synchronous UCB0CTL1…
Part Number: BOOST-TUSS4470 Hello expert,
I ordered TUSS4770 and started to set up the board for the customer meeting.
However, the EVM looks like doesn't work properly...
VDRV is always "0" and there are no images showing up to the measurements &…
Part Number: BOOST-TUSS4470 I purchased the TUSS44x0 EVM and have trouble installing the GUI for the demo application, I get a error message when running the installer. It gives me a network error that the system can't find the MSP430_Driver_Config.lnk…
Part Number: BOOST-TUSS4470 Hello,
I am looking at using an ultrasonic time of flight measurement to characterize a process of making lubricants with various viscosities and additives.
Preferably I would be able to make this measurement from the outside…