Hi, I would like to delete my following post, because in that post I have shared confidential technical data which supposse not to be shared in the public forum.
BOOSTXL-DRV3245AQ1: BOOSTXL-DRV3245AQ1 - Motor drivers forum - Motor drivers - TI E2E support…
Part Number: BOOSTXL-DRV3245AQ1 I have verified that SPI is set up correctly, nFAULT pin is not giving any warnings or faults, and registers are values as expected. I am driving the INH/Lx pins with an ST microcontroller at 30kHz PWM frequency. Please…
Part Number: BOOSTXL-DRV3245AQ1 I am unable to switch a FET on by setting a 3.3V signal on INHA for example.
I powered up the board with 24V, connected 3.3V, GND, nSCS, SDI, SDO and EN pin.
The GHx are around 5.8V. No error indication on nFault or inside…
Part Number: BOOSTXL-DRV3245AQ1 Now when writing the Shunt Amplifier Control Register (80x magnification factor), I didn't calculate its CRC and write it to SPIWR_CRC, which caused the 80x magnification factor to not work. I wonder if the value in the…
Part Number: BOOSTXL-DRV3245AQ1 Other Parts Discussed in Thread: TMS570LS1224 , There is a NDA between Toro and TI.
Cameron Perl, our TI FAE, recommended that I use the E2E forum for the following question.
- I am not able to run a BLDC motor using the…
Part Number: BOOSTXL-DRV3245AQ1 I bought the evaluation board BOOSTXL-DRV3245AQ1 for motor drive, but I cannot find any schs. Could you please support the relevant schematics for application or some chip information of DRV3245AQ1. Thanks.
Part Number: BOOSTXL-DRV3245AQ1 Hi TI-team
My customer wants to buy BOOSTXL-DRV3245AQ1 so please tell me the accessory information.
Are there any accessories at the time of purchase ?
Is it a single board ?
Best Regards,
Koji Hayashi
Part Number: BOOSTXL-DRV3245AQ1 HI
Could you please provide the EVM User Guide, Layout and Schematic Guide? I didn't find them in my secure software. My email is wayne.liu@tii.com
Thanks.
Part Number: BOOSTXL-DRV3245AQ1 I bought the evaluation board BOOSTXL-DRV3245AQ1 for motor drive, but I cannot find any schs. Could you please support the relevant schematics for application.
Thanks,
Ryan
2020/1/13