Part Number: BOOSTXL-DRV8301 Tool/software: Hi all,
I'm attempting to interface with a BOOSTXL-DRV8301 over SPI using an FPGA. I am able to drive a motor, but I am receiving temperature warnings and cannot read the registers otherwise, so I am hoping…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE , DRV8301 , TMS320F28027F , C2000WARE , CONTROLSUITE Tool/software: I am using mc is tms320f28027f and drv8301 to run BLDC motor. I have taken lab example from motorware_1_01-00_18;/sw…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: DRV8301 Can I go above the 24 V supply voltage limit on the BOOSTXL-DRV8301 if it stays under the max of 65 V for the actual DRV8301 chip?
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE Which Motorware variable can return the live/online phase current of BLDC motor while running ?
How can I calculate live Phase current of BLDC motor?
Part Number: LAUNCHXL-F28069M Hi Team,
a PMSM motor with parameter:
pole pairs = 10
rate speed = 180RPM
rate voltage = 36V
Rs = 5.0R
Stator inductance = 27mH
Time constance = L/R = 5.4mS
The customer use lab02b to test the RoverL and Rs,
RoverL = -741…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: BOOSTXL-DRV8301 , DRV8301 , C2000WARE , SFRA , TIDM-02007 , BOOSTXL-3PHGANINV , CONTROLSUITE Hi
I am referring to this post from the E2E-Forum: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE , CCSTUDIO I installed the instaspin universal Gui and it will not run past the l"loading application"screen.
Running Win 10 and copied the .out file to the directory.
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE How a c2000 uC is synching the ADC samples to make sure it is sampling when the low side fet is on? I am following lab guides and foc guides. There is no mention of how adc is synching…
Part Number: BOOSTXL-DRV8301 Hi Team,
Having issues getting MOSFETs to PWM on BOOSTXL-DRV8301 while connected to J5, J6, J7, J8 of LAUNCHXL-F28377S. Using Matlab Simulink to program in LAUNCHXL-F28377S. MOSFETs does not switch for channels PWM2A/B, PWM6A…
Part Number: TMDSCNCD28069MISO Other Parts Discussed in Thread: BOOSTXL-DRV8301 Hi Team,
According to 2.1 Overview of user guide below, TMDSCNCD28069MISO can be paired with BOOSTXL-DRV8301.
But after checking the picture of both I can't find how they are…