Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: DRV8301 Respected Sir/Madam,
Is it safe to drive a BLDC motor with following specifications using the DRV8301 Booster pack ( BOOSTXL-DRV8301 ) and C2000 F28069M piccolo launchpad (LAUNCHXL…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: MOTORWARE Tool/software: Code Composer Studio Which line of the code that update the values of global variables such as, 'gMotorVars.Flag_enableSys', ' gMotorVars.PosStepInt_MRev', ' gMotorVars…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: LAUNCHXL-F28027F , DRV8301 Hello,
I would like to generate a square signal on motor's output of the board BOOSTXL-DRV8301 (A, B and C) with Simulink.
I work with LAUNCHXL-F28027F and BOOSTXL…
That's fine, you can keep the 5V power from both sides without doing anything, Or remove the jumper on JP1&JP2 on LaunchPad that only use the power from Boostxl-drv8301. The latter option is recommended.
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: DRV8301 , MOTORWARE
Tool/software: Code Composer Studio
Dear TI team,
I have a simple project, I chose doing it with TI launchpad instead of Arduino but it seems it will take so much…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: DRV8301 I am using this to test a fan motor, but the motor requires a higher amperage (i.e. 40 amps). I can get it to run at lower speeds restricting the amperage to 15 amps. Is there a suggested…
Part Number: BOOSTXL-DRV8301 Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM , DRV8305-Q1EVM Dear all,
Can this EVM kit (BOOSTXL-DRV8301 +LAUNCHXL-F28207F) control motor as 33,000rpm?
>motor: 4 pole and 3 phase BLDC
>Voltage: 10~14V, Current…
Other Parts Discussed in Thread: BOOSTXL-DRV8301 Hello,
LAunchPadXL TM320F28069M development board BOOSTXL-DRV8301 driver board, running proj_lab13b case, for the first time, the electric control motor will sometimes turn around, and the forward and…
Other Parts Discussed in Thread: BOOSTXL-DRV8301 , LAUNCHXL-F28069M , DRV8301 Hello,
We are using BOOSTXL-DRV8301 and LAUNCHXL-F28069M and want to implement a self-made solidThinking EMBED code. The code was verified and test on our custom made inverter…
Hi Jim,
Are you using the BOOSTXL-DRV8301 Boosterpack for running the motor? If yes, have you referred to the following documents already:
1. BOOSTXL-DRV8301 Quick Start Guide
2. BOOSTXL-DRV8301 Hardware User's Guide
If not, then could you…