Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM Tool/software: I am trying to setup LAUNCHXL-F28379D with BOOSTXL-DRV8305EVM. I will be using MATLAB to further connect it and control motor.
Can anyone please help me…
Hey Oishi-san,
shunsuke.oishi said: Is it safe to assume that the board can output a current at 20A even when a voltage of 45V is applied?
Yes, the current output depends on the load but a 20A load is the maximum current, this board and its components…
Part Number: BOOSTXL-DRV8305EVM Other Parts Discussed in Thread: DRV8305 Tool/software: Hello,
We are using an BOOSTXL-DRV8305EVM booster pack for our motor control applications which has an DRV8305 Motor driver integrated on it. The half-bridge circuit…
Part Number: BOOSTXL-DRV8305EVM Other Parts Discussed in Thread: DRV8305 Tool/software: Hello,
We are using an BOOSTXL-DRV8305EVM booster pack for our motor control applications which has an DRV8305 Motor driver integrated on it. The half-bridge circuit…
Part Number: BOOSTXL-DRV8305EVM Other Parts Discussed in Thread: LAUNCHXL-F28379D Tool/software: Hi Design Support Team,
Hope this email finds you well.
Is BOOSTXL-DRV8305EVM (DRV8305N 3-Phase Motor Drive BoosterPack Evaluation Module) compatible…
Part Number: BOOSTXL-DRV8305EVM Hi,
I'm looking for a document with dimensional information for BOOSTXL-DRV8305EVM. Do you have any information? I would like to use it as a reference when replicating the EVM circuit.
Thanks,
Conor
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM Tool/software: Good Morning
I have a LAUCHXL-F28379D and a BOOSTXL-DRV8305EVM. I would like to use them to drive a PMSM. Are there any examples that will work in the InstaSPIN…
Please take a look at the las user's guide and follow the guide to set up the kits.
Universal Project and Lab User’s Guide: https://www.ti.com/lit/spruj26
jeongin jang said: I am using -Alien Power System APS 5055S Sensed Outrunner Brushless Motor…
Part Number: BOOSTXL-DRV8305EVM Other Parts Discussed in Thread: DRV8305 Hello ,
I have an issue with the BOOSTXL-DRV8305EVM, when I try to run the "3-PWM Mode", it's not working / no output on the driver.
The following steps have been done:
After…
Part Number: BOOSTXL-DRV8305EVM At BOOSTXL-DRV8305EVM the REF pin is connected to 3.3V, this gives offset of 1.65V (when k=2) to the Current Senses.
But for low-side current sensing we never have negative current, right?
Current always goes with…