Hi Simon,
The DRV8308 is typically intended for starting a motor and running it. It was not intended for quick stops and starts.
May I suggest you consider the DRV832x series of device? These devices do not have the algorithm, so you can either add…
Hello na na78,
Since you are able to use the BOOSTXL-DRV8320H EVM to spin the motor with the sensorless configuration, I'm wondering if there is an issue with the Hall sensor connections. Are the power and ground pins for the Hall sensors connected properly…
To all posters looking for the TIDA-00735 code:
The code for this reference design cannot be located. We apologize for this inconvenience.
Similar code using the MSP430F5529 is available for the BOOSTXL-DRV8320H/S ( www.ti.com/.../slvc683 )
There are…
Part Number: MCT8316Z Other Parts Discussed in Thread: DRV8329 , DRV8328 , DRV8300 , DRV8308 , DRV8320 , DRV8320R , DRV8323R , DRV8323 , MOTORWARE Hello,
I am finding BLDC motor controller and found the 8316 series.
Looks like good one but I have some questions…